We are currently using CY7C64315-16LKXIT
----------------------------------------
We are working on programming these chips through a microcontroller, instead of using a programmer header as done on previous projects using this part. We have run into a couple of issues and would like to pass on some questions to Cypress.
1. What is the best protocol for programming the CY7C64315 device with a microcontroller? Right now we are working on programming them with the ISSP protocol, going off information found in AN44168
2. Is there a version of the ISSP source code that explicitly supports CY7C64315?
3. If not, what are the parameters/vectors needed by CY7C64315 that needs to be set in the HSSP_CY8Cxxxx source code? We see some information for CY7C64215, how compatible is this with CY7C64315?
--------------------------------------------
Solved! Go to Solution.
Hi,
Please find the attached project. This supports HSSP for CY7C64315. AN59389 was modified to support HSSP for enCore V devices.
Following are a few points to note about the project:
1. The project writes 0xB9 to the entire flash and sets flash security to "U" for all blocks.
2. Table below shows the connections between Host and target
SIGNAL HOST TARGET
---------------------
SDATA P1.2 P1.0
SCLK P1.3 P1.1
XRES P0.0 XRES
PWR P0.1 Vdd
TP P0.7 n/a
3. Right now "powercycle" mode of programming is enabled. Uncomment the #define on line61 in issp_directives.h to use "Reset Mode".
4. The project is developed for CY8C29866-24AXI.
5. The LCD can be connected to Port2 to see the status of programming (displayed on line0) and read SiliconID(displayed on line1). Refer LCD user module datasheet for LCD connections.
6. Erase EncoreV flash using "PSoC Programmer software". Then program EncoreV using HSSP. Use PSoC Programmer to read EncoreV again to verify if the flash was actually written.
Regards,
Hemanth