- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I would like to know if the CY3686 which is the NX2LP-Flex development kit includes the FX2LP development kit (CY3684)?
If it is the case, will the CY3686 be delivered with all the sources and firmwares for the two microcontrollers (FX2LP and NX2LP-Flex)?
We would like to develop a USB application but we do not know which one to use, if the CYCY86 is including the CY3684 then we will directly order the CY3686 and try the two USB microcontrollers.
Thank you in advance for your answer.
Jamal.
- Labels:
-
ispn:39563:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Yes CY3686 is combination of CY3684 hardware and Addon board for mounting the NAND. Also you get the sources and firmware examples of CY3684. So you can directly order CY3686. Even the firmware for NX2LP-Flex will be tested using the CY7C68013A chip.
-Gopal