- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I'm a USB newbie and try to do something useful with the 100 pin CY7C68013A on an old FPGA dev board. While following the example for the bulk loop program on linux (AN73609), the program complains about too many endpoints. Is the example not applicable to my device or did I catch the wrong firmware?
Thanks,
Felix
Enter the choice [e.g 3] :1
----------------------------------------------------------------------------------------
Number of interfaces 1
Number of alternate settings 1
interface Number 0, Alternate Setting 0,Number of Endpoints 4
EP Address 2 Bulk OUT Endpoint
EP Address 4 Bulk OUT Endpoint
EP Address 86 Bulk IN Endpoint
EP Address 88 Bulk IN Endpoint
----------------------------------------------------------------------------------------
What do you want to do ?
1. Give information about the device.
2. Do the bulk transfer
3. Exit
Enter the choice [e.g 3] :2
-------------------------------------------------------------------------------------------------
This function is for testing the bulk transfers. It will write on OUT endpoint and read from IN endpoint
-------------------------------------------------------------------------------------------------
Found FX2LP bulkloop device, continuing...
to many Endpoints
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Please let us know which firmware you are using? Is it the one along with the AN?
Regards,
Gayathri