This widget could not be displayed.
Anonymous
Not applicable
Mar 03, 2014
06:08 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 03, 2014
06:08 PM
The CY7C68013 is a 3.3V device. The "features" page of the manual says that its inputs are "5V tolerant", but the "absolute maximums" chapter is somewhat ambiguous - it says 5.25V for inputs and Vcc+0.5V for outputs in high-Z state. Every bi-directional port pin, when used as an input, is also an output in high-Z state, so I'm not sure... any help would be appreciated.
0 Replies
This widget could not be displayed.