Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

Anonymous
Not applicable
        Hi, Guys:   
I am using the stand alone NX2LP-Flex board(taken from the CY3686 kit and the board is populated with CY7C68033 for U1) to use Samsung's K9HBG08U1M or K9WAGo8U1A, both chips are 2k/page nand flash. I have encountered the following problem:   
1) the NX2LP Programmer Utility stopson "identifing device", no pop-up dialogs come up as expected to allow me to add nand chip profiles. Why this machine does not pop up the "add new part" dialog?   
2) I then use a second PC which can go untill to pop up the "add new part" dialog. Then I added the new parts as required and restarted the NX2LP Programmer Utility. the device can be identified. But when programming button is pressed, the utility reports "FAT32 formatting failed.."   
0 Likes
2 Replies
Anonymous
Not applicable

 I am having the same issue..

0 Likes
Anonymous
Not applicable

 Hi Sachin,

   

 

   

Which Nand flash are you using? Is it the same as the ones mentioned in the post above? 

   

Can you just try with a different sample of the Nand flash, just to figure out if it is a Nand issue.

   

 

   

Regards,

   

Gayathri

0 Likes