Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

 Doing a host computer and FPGA communication, through cy7c68013 of GPIF_FIFO read and write to communications, the following initialization of the firmware is 68013, help me find out where the problem, I have engaged in several days, and specific settings are as follows:
// EP2OUT, bulk, size 512, 4x buffered,autoout,byte
// EP6IN, bulk, size 512, 4x buffered,autoin,byte

note:the code belowed acomplishes the "gpif fifo write" part
Code:

   

void TD_Init(void)             // Called once at startup
{
  // set the CPU clock to 48MHz
  CPUCS = ((CPUCS & ~bmCLKSPD) | bmCLKSPD1);
  GpifInit (); // initialize GPIF registers
  
  SYNCDELAY;
  EP2CFG = 0xA0;     // EP2OUT, bulk, size 512, 4x buffered
  SYNCDELAY;                    
               
  EP6CFG = 0xE0;     // EP6IN, bulk, size 512, 4x buffered
  SYNCDELAY;                    

  FIFORESET = 0x80;            // activate NAK-ALL to avoid race conditions
  SYNCDELAY;                    //
  FIFORESET = 0x02;            // reset, FIFO 2
  SYNCDELAY;                    //
  FIFORESET = 0x06;            // reset, FIFO 6
  SYNCDELAY;                    //
  FIFORESET = 0x00;            // deactivate NAK-ALL
  SYNCDELAY;                    //


  EP2FIFOCFG = 0x10; // auto out mode, disable PKTEND zero length send, byte ops
  SYNCDELAY;
  EP6FIFOCFG = 0x08; // auto in  mode, disable PKTEND zero length send, byte ops
  SYNCDELAY;   
  // out endpoints do not come up armed
  // since EP2OUT is quad buffered we must write dummy byte counts four times
EP2BCL = 0x80;     // arm EP2OUT by writing byte count w/skip.
  SYNCDELAY;                    
  EP2BCL = 0x80;
  SYNCDELAY;                    
  EP2BCL = 0x80;
  SYNCDELAY;
  EP2BCL = 0x80;
  SYNCDELAY;  
  
}
 In TD_Poll () the code below, there is a problem here, doesn't the cpu process in the autoout way?Why the cpu process here? And I don't  understand the following code, and do not know whether the code is correct or not .I found this code in a paper. I hope someone can explain the code,thanks! 

   

void TD_Poll(void)
{
//      完成FIFO的写操作,从EP2-OUT写到外部FIFO中

   

// finish the fifo writing,from EP2 to external fifo
/*****************************************************************************/
if ( ! ( EP2468STAT & bmEP2EMPTY ) )
{
  SYNCDELAY;
  EP2BCL=0x00;
//SKIP=0,这里不就是手动在处理数据吗??为什么,autoout是什么意思呢?
  }  

  if(GPIFTRIG & 0x80)
  {
   if(!(EP24FIFOFLGS & 0x20))
   {
     GPIF_SetAddress(ADDRESS_FIFO1);   //设置地址
     GPIFTCB0=EP2FIFOBCL;
     SYNCDELAY;
     GPIFTCB1=EP2FIFOBCH;
     SYNCDELAY;
     GPIF_FIFOWrite(0);     //触发FIFO写波形
   }
  }
Also: I see the <ez-usb trm > there that should be added in the initialization
REVCTL=0x03; 
I do not know why?

0 Replies