Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

This widget could not be displayed.
Anonymous
Not applicable

1,question about function "ept->Read(&buf, bytestosend);" in control transfer

   

after running the code “ept->Read(&buf, bytestosend);”,Has the transfer ended?

   

it's vital to know the answer in continous control transfer while repeated inquring a status variable through control transfer.

   

 

   

 

   

2,question about large bulk transfer

   

in a case that a DSP transmit an image to the host by using bulk transfer, the image has 1447680 bytes,so can the bulk transfer code be executable as below:

   

OVERLAPPED  inOvLap;

   

inOvLap.hEvent   = CreateEvent(NULL, false, false, "CYUSB_IN");

   

LONG  length =1447680; 

   

USBDevice->EndPointCount(); 

   

BulkInEpt=(CCyBulkEndPoint *) USBDevice->EndPoints[1];

   

UCHAR  *inContext = BulkInEpt->BeginDataXfer(inBuf, length, &inOvLap); 

   

BulkInEpt->WaitForXfer(&inOvLap,1000); 

   

BulkInEpt->FinishDataXfer(inBuf, length, &inOvLap,inContext); 

   

CloseHandle(inOvLap.hEvent);  

0 Likes
1 Reply
This widget could not be displayed.
Anonymous
Not applicable

1. Yep. You will have to look at the returned bool value to see whether the transfer succeeded or failed.

   

2. Yep. It should work. The timeout value you are providing seems small.

   

Regards,

   

Anand

0 Likes
This widget could not be displayed.