Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

hi,

   

I'm using  two bladerf (tx and rx) to transfer continuous data from  tx to rx and i want to recuperate data stored in the fx3(rx) mcu in my computer . I was wondering which is the best program that allows me to do so ? 

   

 what I want to do is to save the data I get on the computer and use it to draw a graph (on matlab) and I need the graph drawing to be real time transfer 

   

can anyone help me plz by providing the suitable link of a source code example (firmware and host application)?

   

Best Regards,

   

mariem

0 Likes
1 Solution
Anonymous
Not applicable

If you are using Matlab, you can use the cyusb.dll library along with Matlab to create the host application. Also, you can refer the Slavafifo project for the firmware.

   

Regards, 

   

- Madhu Sudhan

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

If you are using Matlab, you can use the cyusb.dll library along with Matlab to create the host application. Also, you can refer the Slavafifo project for the firmware.

   

Regards, 

   

- Madhu Sudhan

0 Likes