Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB hosts hubs transceivers Forum Discussions

Sort by:
Koki
USB hosts hubs transceivers
Hello Support,   My customer want to use HX2LP. Can you tell me the recommended pattern for HX2LP? Best regards, Koki Show More
Augustine_Yeh
USB hosts hubs transceivers
Hi Infineon Can you tell us which one is 3.3 V/SS PHY pin in CYUSB3314-BVXI/100pin , We need additional ferrite bead is required to isolate , Thanks!!... Show More
hobi_4669811
USB hosts hubs transceivers
So, i need to save raw datas (raw 8 bit, YCpCr 4.2.2 ) coming from a camera (USB 3.0 UVC+CDC)into a standard UDISk (USB 2.0 HS or USB 3.0 MSD). The CD... Show More
abhip
USB hosts hubs transceivers
Hello Folks,   I am working with Cypress c# streamer to receive the images. The application is streaming continuously without any failures. But I am n... Show More
shamshu
USB hosts hubs transceivers

Unable to find the the Footprint and Land Pattern for the part number : CYUSB4357-BZXC 

DaEr_349131
USB hosts hubs transceivers
Hi, the datasheet reads: > After TetraHub is configured in a high speed system, it is in single TT mode. The host may then set the hub into multipl... Show More
BhargavGolla
USB hosts hubs transceivers
Hello, I am facing Controller hang during SPI data transfer, through uart prints i was able to see function is entering into the SPi wrapper function ... Show More
tbo
USB hosts hubs transceivers

在使用CY7C65213A时,碰到一些问题,麻烦解释下,谢谢!!

Roman-N
USB hosts hubs transceivers
Hello, We are currently in development of a product implementing HX3 CYUSB3304 USB hub. We set the hub as I2C slave to be configured from an external ... Show More
Augustine_Yeh
USB hosts hubs transceivers
Hi Infineon Which OS and Systems can support for CYUSB3314-88LTXI? Is it include Raspberry Pi (HW/OS)/Apple/Linux too, Thanks! Raspberry Pi (HW) ... Show More
Forum Information

USB hosts hubs transceivers

Discussion forum regarding USB hosts hubs and transceivers topics.