Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB hosts hubs transceivers Forum Discussions

Roman-N
USB hosts hubs transceivers
Hello, We are currently in development of a product implementing HX3 CYUSB3304 USB hub. We set the hub as I2C slave to be configured from an external ... Show More
Augustine_Yeh
USB hosts hubs transceivers
Hi Infineon Which OS and Systems can support for CYUSB3314-88LTXI? Is it include Raspberry Pi (HW/OS)/Apple/Linux too, Thanks! Raspberry Pi (HW) ... Show More
Marcelo_Macedo1
USB hosts hubs transceivers
Hi, Can you please advise if  the upstream port for HX3PD could be dual role, sink and source? I could just find this old post during early stage of t... Show More
dl2mkx
USB hosts hubs transceivers
I'm currently reading back and forth the Datasheet, AN91378 and EVB CY4613 schematics but was not able to find:  If not using pin strapping and go wi... Show More
tomasalar
USB hosts hubs transceivers
Hello forum, I am trying to use the CYUSB3324 with one port Type C for US and one for DS, the other ports are Type-A and SD card reader. My complicati... Show More
Wellington
USB hosts hubs transceivers
Hi Cypress We have Two FX3 connect to HX3PD hub design in our system board. The goal is to stream data on both FX3 at the same time. The issue we seen... Show More
dl2mkx
USB hosts hubs transceivers
Hi,in our application the HX3 would be connected to an embedded SOM (iMX8+) and I need one shared port (USB2 for Touch + USB-SS for a data capture car... Show More
qin
USB hosts hubs transceivers
In the CYUSB332x system diagram, can the ARM Cortex-M0 CPU control the SS control to process data from the device end
qin
USB hosts hubs transceivers

In the EZ-USBHX3PD system diagram, can the ARM Cortex-M0 CPU control the SS control to process data from the device end

prenstrong
USB hosts hubs transceivers

使用默认配置(pin-strap悬空),DSx_PWREN不拉低(PWR_SW_POL接1k电阻到地),量到IC的3.3V、1.2V、26MHz信号都OK,是什么原因呢?

信息安全,上不了图

Forum Information

USB hosts hubs transceivers

Discussion forum regarding USB hosts hubs and transceivers topics.