Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB hosts hubs transceivers Forum Discussions

Koki
USB hosts hubs transceivers
Hello support, Thank you for your usual support. I have a question of CYUSB3304.  Are there any concerns about setting the RESETN input to L while the... Show More
NoAr_1540581
USB hosts hubs transceivers
Hello   Q1) If they only set the MODE_SEL pin to "1.1" (without external EEPROM), will it be possible to use "internal ROM configuration" and use it a... Show More
jwr152
USB hosts hubs transceivers
I currently have 2 DELL model computers that are same Latitude 5430 systems with Windows 10 Enterprise. I've been successful installing driver package... Show More
Translation_Bot
USB hosts hubs transceivers
    HX3 has pins to connect to power switch enable pin and over-curret flag pin. We have a question about polarity of those enabled pins and over-curr... Show More
Koki
USB hosts hubs transceivers
Hello Support, The following Microchip USB hubs have a host switching function called FlexConnect. https://ww1.microchip.com/downloads/en/Appnotes/AN1700-FlexConnect-Applications-00001700D.pdf... Show More
P_Pieters
USB hosts hubs transceivers
Do these voltage thresholds apply to the SELFPWR and RESET# pins?   Asked differently, is a pull-up voltage of 3.3V sufficient? In our application, t... Show More
PAUL27
USB hosts hubs transceivers
  We are working on a home telephone project. For that we are looking for two types of solution    1.which contains USB3.0 to ethernet output and one ... Show More
Koki
USB hosts hubs transceivers
Hello Suopport,   Regarding the GPIO AC specifications, it seems that the maximum and minimum values of rise/fall time are the same in Fast mode and S... Show More
Abi
USB hosts hubs transceivers
Hi I am using CYUSB4357-BZXC Hub IC with US as Type C port and DS1 and DS2 as Type C port and DS6 and DS7 as usb2 ports. how can i disable PD functi... Show More
KyleLin
USB hosts hubs transceivers
Hi, What is "Tc" and "Thermal loss(watt)" of CYUSB3314-88LTXI? Customer needs these data to conduct thermal simulation. Regards, Kyle Show More
Forum Information

USB hosts hubs transceivers

Discussion forum regarding USB hosts hubs and transceivers topics.