Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

TeMa_2997106
Level 6
Level 6
10 likes received 10 solutions authored 250 replies posted

If the upstream of HX2LP is HS and the downstream is connecting HS, FS, LS USB devices, are there any specification restrictions?

Are there any restrictions (differences) in the specifications when communicating with FS and LS at the same time and when communicating alternately after a certain period of time?

In the current application, the upstream is FS, so there is no problem with SingleTT.
In a new application, upstream will be HS, so I would like to confirm if there are any specification restrictions.

Thanks,
Tetsuo

1 Solution
MallikaK_22
Moderator
Moderator
Moderator
250 solutions authored 500 replies posted 250 replies posted

Hi Tetsuo,

Could you please elaborate on your question? I didn't understand the question on specification restrictions.

Meanwhile, you may take a look at this App Note if it answers your query.

Regards,

Mallika

View solution in original post

0 Likes
5 Replies
MallikaK_22
Moderator
Moderator
Moderator
250 solutions authored 500 replies posted 250 replies posted

Hi Tetsuo,

Could you please elaborate on your question? I didn't understand the question on specification restrictions.

Meanwhile, you may take a look at this App Note if it answers your query.

Regards,

Mallika

0 Likes
TeMa_2997106
Level 6
Level 6
10 likes received 10 solutions authored 250 replies posted

Mallika-san,

I want to know "connectivity".

In SingleTT, when US is HS and DS is HS / FS / LS devices are connected, are there any of these three devices that cannot communicate?

I think that it possible use cases are:
Is there any applicable one?

1) When HS, FS, and LS devices are connected to the Downstream, communication with all (HS, FS, LS) devices becomes impossible.
2) HS device can communicate, but simultaneous communication to FS and LS devices is not possible.
3) Communication with LS device is not connected only during communication with FS device
4) In the case of simultaneous communication to FS and LS, the speed is pulled to the LS side, so the throughput drops but communication is possible.

If it is in the above case 1/2/3 state, is there any way to recover? If so, what should I do?
(device re-insertion / HUB reset required / communication alternately / etc..)

Thanks,
Tetsuo

0 Likes
TeMa_2997106
Level 6
Level 6
10 likes received 10 solutions authored 250 replies posted

Do you have any other comments on this thread?

Tetsuo

0 Likes
MallikaK_22
Moderator
Moderator
Moderator
250 solutions authored 500 replies posted 250 replies posted

Hi Tetsuo,

Apologies for the delay in response.

In case more than 1 low/full speed devices are connected in the downstream ports, it is bound to affect the USB performance. 

Kindly refer to this KBA .

Regards,

Mallika

0 Likes
TeMa_2997106
Level 6
Level 6
10 likes received 10 solutions authored 250 replies posted

Mallika-san,

Thank you for your comment.

I understand.

 

Thanks,

Tetsuo

0 Likes