Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NoAr_1540581
Level 5
Level 5
Distributor - Macnica (Japan)
5 solutions authored 250 sign-ins 100 replies posted

Hello

I will operate DRP(Dual role port)  using the UP stream port and DS1 (PD support port) of HX3PD.

Is it possible to operate DRP(Dual Role Power) and DRD(Dual role Data) between US and DS1?

If yes, are there any special control?

Best Regards

Arai

0 Likes
1 Solution
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello Arai-san,

Please refer to the ordering information section in the datasheet, in HX3PD the US port is a DRP and DS1 port is a DFP.

So, it wont be possible to change the configuration to be a DRP port on DS1 since the Rd terminations arent supported.

The default firmware has the US port configured as a device and DS1 as a host and since the ports are as per the hub controller, the configuration should not be changed to DRD port.

Best Regards,
Sananya

View solution in original post

0 Likes
1 Reply
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello Arai-san,

Please refer to the ordering information section in the datasheet, in HX3PD the US port is a DRP and DS1 port is a DFP.

So, it wont be possible to change the configuration to be a DRP port on DS1 since the Rd terminations arent supported.

The default firmware has the US port configured as a device and DS1 as a host and since the ports are as per the hub controller, the configuration should not be changed to DRD port.

Best Regards,
Sananya

0 Likes