Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB hosts hubs transceivers Forum Discussions

TeMi_4035936
Level 1
Level 1
5 sign-ins First like received First reply posted

I was asked about USB2.0 Hub CYUSB2304-68LTXI.

1. What is the actual threshold of VHSDSC(Disconnection Envelope Detector)?

   They know that the min & max VHSDSC values described in the USB2.0 specification are 525mV and 625mV.

   They need to know the actual threshold which is actually configured or characterized for CYUSB2304.

2. Is it possible for customers to adjust the VHSDSC?

0 Likes
1 Solution
HirotakaT_91
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Hi,

A1. We can just say HX3 (CYUSB2304) meets its requirement. That is, VHSDSC is between 525 mV and 625 mV.

We might be able to show the actual value, but note that system must work irrespective of the HX3's VHSDSC value which within a range of 525mV-625mV.

A2. No, it is definitely not.

Best regards,

Hirotaka Takayama

View solution in original post

0 Likes
4 Replies
HirotakaT_91
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

Hi,

A1. We can just say HX3 (CYUSB2304) meets its requirement. That is, VHSDSC is between 525 mV and 625 mV.

We might be able to show the actual value, but note that system must work irrespective of the HX3's VHSDSC value which within a range of 525mV-625mV.

A2. No, it is definitely not.

Best regards,

Hirotaka Takayama

0 Likes

Takayama-san

Thank you for your reply.

and sorry in Japanese.

顧客(当社顧客)は、御社のHub ICではないですが、END Customerにおいて、他メーカー製品でUSB通信不良が発生しているようで、

ENDの車メーカーより御社の製品にかんしても問題が発生しないことを確認するよう依頼がきているのが

今回の問合せの背景になります。

頂いた内容ベースで回答しておりますが、HX3'sの設定電圧(We might be able to show the actual value)の

回答依頼を強く頂いております。

ご対応頂けますと幸いです。

以上、

0 Likes

Hello,

Cypress HX3のVHSDSCは、USB 2.0 Specに従い、525mV-625mVに収まっております。

Specに従っているため、繰り返しになりますが、お客様としてはこのrange内であればいかなる場合でも動作させる必要があり、このrange内で問題が発生していてもCypress側で何かしら責任を取ったり、チップを作り直すような対応は致しません。

また、具体的なCharacterization情報は、申し訳ございませんが提供できかねます。

よろしくお願い致します。

Hirotaka Takayama

0 Likes

Hi, tanakayama san

ご回答しにくい内容にご返信いただきありがとうございます。

以上、今後ともよろしくお願いします。

0 Likes