Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cwchc_3277416
Level 1
Level 1

Specified in data sheet: pull-down resistor of greater than 100k is required for individual mode (pin 39 of HX2VL)

pastedImage_6.png

Also specified in data sheet: maximum leakage current is 10uA

pastedImage_5.png

The maximum leakage current will result in 1V drop on the pull-down resistor. This 1V level might not be interpreted as logic low since input low voltage of 0.8V (max) is not met.

In this case, what is Cypress recommendation to guarantee the design at worst case? 

What will be the side effect if a pull-down resistor of let's say 75kR is used for Gang/Individual pin? 

Kindly enlighten. 





1 Solution
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

The maximum leakage currents mentioned in the datasheet are worst case scenarios and should not cause a drop as large as 1V. We will look into the exact measured characteristics and update the datasheet if needed.

Best Regards,

Sananya

View solution in original post

0 Likes
1 Reply
Sananya_14
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

The maximum leakage currents mentioned in the datasheet are worst case scenarios and should not cause a drop as large as 1V. We will look into the exact measured characteristics and update the datasheet if needed.

Best Regards,

Sananya

0 Likes