Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PaKu_3818476
Level 1
Level 1
First like given

I am new to this C#. I want a C# program to transfer Data from FPGA to PC. I tried using Bulkloop_VCS it is not working may be I have to make some changes but I have No Idea How the Bulkloop_VCS Program written so If any one worked in this please share it . it makes easy for me.SrinathS_16

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello,

Please refer to Cypress provided Streamer and Control Center source code for implementation of data transfer using the C# XferData() API. These source codes are present as part of the FX3 SDK.

- Streamer host application requires that the firmware running on the device could continuously read data (IN endpoint) or continuously provide data (OUT endpoint).

- Bulkloop host application requires that the firmware running on the device is capable of looping back the data received on a OUT endpoint onto an IN endpoint.

- Control Center can be used to perform any sequence of read/write onto the device.

Best regards,

Srinath S

View solution in original post

0 Likes
1 Reply
SrinathS_16
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello,

Please refer to Cypress provided Streamer and Control Center source code for implementation of data transfer using the C# XferData() API. These source codes are present as part of the FX3 SDK.

- Streamer host application requires that the firmware running on the device could continuously read data (IN endpoint) or continuously provide data (OUT endpoint).

- Bulkloop host application requires that the firmware running on the device is capable of looping back the data received on a OUT endpoint onto an IN endpoint.

- Control Center can be used to perform any sequence of read/write onto the device.

Best regards,

Srinath S

0 Likes