Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB hosts hubs transceivers Forum Discussions

mame_1363116
Level 2
Level 2
Welcome!

I am designing an USB 3.0 hub. Since I will use just 3 ports is can I power the system using the 5V coming from the VBUS of the host without needing an external power source? Obviously the 5V will go in voltage regulator to obtain the 3.3V and 1.2V for the IC.

0 Likes
1 Solution
Anonymous
Not applicable

Hello,

First of all, VBUS (5V) coming from the Host is required for the Hub to detect the connect/disconnect status for non-embedded Hubs.

It is possible to obtain 3.3V and 1.2V from VBUS, but it can power HX3 IC but cannot provide sufficient power to the downstream connected devices. So, it is recommended to use self powered Mode for USB3.0 Hubs.

Please refer "Power Consumption" section in the HX3 datasheet at http://www.cypress.com/file/141031/download 

which lists the power consumption of the HX3 in different cases.

And for your reference, USB3.0 Host can provide only 900mA@5V.

Regards,
Anil

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hello,

First of all, VBUS (5V) coming from the Host is required for the Hub to detect the connect/disconnect status for non-embedded Hubs.

It is possible to obtain 3.3V and 1.2V from VBUS, but it can power HX3 IC but cannot provide sufficient power to the downstream connected devices. So, it is recommended to use self powered Mode for USB3.0 Hubs.

Please refer "Power Consumption" section in the HX3 datasheet at http://www.cypress.com/file/141031/download 

which lists the power consumption of the HX3 in different cases.

And for your reference, USB3.0 Host can provide only 900mA@5V.

Regards,
Anil

0 Likes