Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
NoAr_1540581
Level 5
Level 5
Distributor - Macnica (Japan)
5 solutions authored 250 sign-ins 100 replies posted

Please find attached.When they checked the rising waveform of the GANG pin, it dropped to the low level.However, since there is no problem with the rise of the 3.3V waveform , they are thinking that something has happened inside and the GANG input signal has dropped. Q) Could you please tell me the causes and mechanisms?

Best Regards

Arai

0 Likes
1 Solution
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

A single pin is used to set  individual  /  gang mode as well as output the suspend flag. This is done to reduce the pin count.

The individual or gang mode is decided within 20 µs after power on reset. It has a setup time of 1ns. 50 to 60ms after reset, this pin is changed to output mode. CY7C65642 outputs the suspend flag, once it is globally suspended. Pull-down resistor of greater than 100K is needed for Individual mode and a pull-up resistor greater  than  100K  is  needed  for  Gang  mode.

See this feature described in the datasheet.  Also, check whether this is what the customer sees in the waveform.

Best regards,

Hirotaka Takayama

View solution in original post

0 Likes
1 Reply
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

A single pin is used to set  individual  /  gang mode as well as output the suspend flag. This is done to reduce the pin count.

The individual or gang mode is decided within 20 µs after power on reset. It has a setup time of 1ns. 50 to 60ms after reset, this pin is changed to output mode. CY7C65642 outputs the suspend flag, once it is globally suspended. Pull-down resistor of greater than 100K is needed for Individual mode and a pull-up resistor greater  than  100K  is  needed  for  Gang  mode.

See this feature described in the datasheet.  Also, check whether this is what the customer sees in the waveform.

Best regards,

Hirotaka Takayama

0 Likes