About designing with CY7C65634-48AXCT

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
NoAr_1540581
Level 5
Level 5
Distributor - Macnica (Japan)
5 solutions authored 250 sign-ins 100 replies posted

Q1) Please tell me the unused pin processing below?
· Test I2C_SCL -> open?
· OVR # [1] - [4] -> open?

· PWR # I2C_SDA -> open?


Q2) Is the recommended pull-up/pull-down value of SELFPWR, GANG pin 10 kΩ correct?

Q3) The would like to know about the state of each terminal during reset, couldyou please share the list?

Q4) Please tell me the internal equivalent circuit of the RESET#pin (in addition, it is included the protective diodes)

Q5) Please tell me the internal equivalent circuit of the "open draininput pin" in datasheet page19?

Best Regards

Arai

0 Likes
1 Solution
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

A1)

These are able to open since  Pad internal Pull Down Resistor or  Pad internal Pull Up Resistor is inside.

A2)

Pull-down resistor of greater than 100K is needed for Individual mode and a pull-up resistor greater  than  100K  is  needed  for  Gang  mode.

Please refer to HX2VL datasheet.

A3)

I am sorry, but what do you mean? Would you like to know the detailed reset sequence? Please clarify.

A4, A5)

Basically, we do not offer internal circuit.

NOTE: Kindly do not post a lot of question in one thread.

Best regards,

Hirotaka Takayama

View solution in original post

0 Likes
4 Replies
HirotakaT_91
Moderator
Moderator
Moderator
500 replies posted 250 replies posted 100 replies posted

A1)

These are able to open since  Pad internal Pull Down Resistor or  Pad internal Pull Up Resistor is inside.

A2)

Pull-down resistor of greater than 100K is needed for Individual mode and a pull-up resistor greater  than  100K  is  needed  for  Gang  mode.

Please refer to HX2VL datasheet.

A3)

I am sorry, but what do you mean? Would you like to know the detailed reset sequence? Please clarify.

A4, A5)

Basically, we do not offer internal circuit.

NOTE: Kindly do not post a lot of question in one thread.

Best regards,

Hirotaka Takayama

0 Likes

A3)

We do not have such a list, so far.

Why the end customer needs these information?

The power on reset can be triggered by external reset or internal circuitry. The internal reset is initiated, when there is an unstable power event for silicon’s internal core power(3.3V).

The internal reset is released after approximately 2.7 micro-seconds of stable internal core voltage. The external reset pin continuously senses the voltage level (5V) on the upstream VBUS. In the event of USB plug/unplug or drop in voltage, the external reset is triggered.

After releasing a reset, chip will be initial state.

Best regards,

Hirotaka Takayama

0 Likes
NoAr_1540581
Level 5
Level 5
Distributor - Macnica (Japan)
5 solutions authored 250 sign-ins 100 replies posted

Takayama san

A3)

It is because their plan to connect PWR # etc to external circuit, so they want to check if there is something unstable during resetting. Is it possible to explain about the state of each terminal( other than reset pin)  during reset even though Cypress does not have such a list.

Best Regards

Arai

0 Likes

Which reset are you talking about? Power ON Reset or external reset?

As a premise, power on reset is used for stabling pins.

Do not use pins before being released. Because pins are unstable.

After Power ON Reset, RDN or RUP Type pins are set to Low or High.

Other pins settings would be depended on customer circuit.

Please let me know which pins or flow you are concerned?

Best regards,

Hirotaka Takayama

0 Likes