- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is it possible to send windows file from PC to FX3 DVK REV3 board on usb3.0 ??
as per cyusb. pdf
The CYUSB3.SYS driver is licensed for distribution ONLY with Cypress USB products and
products that employ Cypress USB chips.
CYUSB3.SYS is a USB device driver for 32 bit Windows XP, 32/64 bit Windows Vista, 32/64 bit
Windows 7 and 32/64 bit Windows 8 Beta that is capable of communicating with any USB 2.0 and
USB3.0 compliant devices. The driver is general-purpose, understanding primitive USB commands, but
not implementing higher-level, USB device-class specific commands. For this reason, the driver is not
capable, for instance, of interfacing a USB mass storage class device to the Windows file system.
Please note that this release doesn't include the USB3.0 bulk streaming interface.
and one more thing is it possible to do the same in case of FX3 board configured as a usb2.0?? because winxp must have installed HID & MASS storage classes driver