- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all
I am working on CYUSB3KIT-003 kit with image sensor ov7675 currently, and using AMCap on PC
I follow the instruction AN75779, and made some modify with the previous discussion
Re: Cypress EZUSB FX3 to stream video from OV7670
AN75779 modification - FX3 for streaming image sensor data
Hardware setting:
ov7675 is initialized by another device, so i2c function on fx3 is disabled
only connect DQ[0-7] PCLK FV LV to fx3
since ov7675 default resolution is 640*480 so I connect the fx3 to usb 2.0 port on PC,
according to the AN75779, the uvc will switch to 640*480 automatically, and AMCap recognize this as well
I enable the #define DEBUG_PRINT_FRAME_COUNT to check the status of frame receiving
and using oscilloscope to check the FV and LV existing, and it does
but i can't see any image on AMCap
the debug info:
most of the time:
UVC: Completed 0 frames and 0 buffers
UVC: Completed 0 frames and 0 buffers
UVC: Completed 0 frames and 0 buffers
UVC: Completed 0 frames and 0 buffers
sometimes:
Application Started
UVC: Completed 0 frames and 0 buffers
UVC: Completed 175 frames and 0 buffers
UVC: Completed 363 frames and 0 buffers
UVC: Completed 528 frames and 0 buffers
UVC: Completed 727 frames and 0 buffers
UVC: Completed 898 frames and 0 buffers
UVC: Completed 1065 frames and 0 buffers
UVC: Completed 1221 frames and 0 buffers
UVC: Completed 1421 frames and 0 buffers
UVC: Completed 1583 frames and 0 buffers
DMA Reset Event: Commit buffer failure
Application Stopped
is anyone encounter the same problem?
Solved! Go to Solution.
- Labels:
-
ispn:38621:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all
Finally I got it work. It turns out the PCLK signal problem. I just change a way to connect PCLK between sensor and FX3
However I can't tell the different of PCLK between two connection ways on oscilloscope.
By the way, during the debugging I add debug message in: uvc.c function CyFxUvcApplnDmaCallback()
which will result in system crash.