cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

jawu_4351971
New Contributor II

in this link https://community.cypress.com/thread/35257?start=0,you said "nothing (MIPI/GPIF II block) will interfere with control of these GPIOs (17,18,19, and 20)."

Now I have use the three GPIO as general IO,and I also use GPIF to receive camera stream,Is this okay?

0 Likes
1 Solution
JayakrishnaT_76
Moderator
Moderator

Hello,

Please note that the MIPI/GPIF will not interfere with the controls of GPIOs 17,18,19,20. So it is perfectly okay to use GPIOs 17,18,19,20 while using GPIF to receive camera stream. The only thing to be noted is that you need to override GPIO17-20 to use them.

Best Regards,

Jayakrishna

Best Regards,
Jayakrishna

View solution in original post

0 Likes
7 Replies