Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

itayc
USB superspeed peripherals
Hi, Is there a way to assign a unique product descriptor and serial number descriptor to each CX3? I prefer to use the DIE_ID as the unique identified... Show More
rossi
USB superspeed peripherals
In my usb2.0 host firmware test, I found something weird. These are some code snippets and the resulting logs.         static void CyFxHostXferCb (uin... Show More
Bashar
USB superspeed peripherals
Our application sends Alt DP video over a USB-C interface. We are trying to use an FX3 processor to be the USB host and enumerate a COTS display drive... Show More
NTaub
USB superspeed peripherals
I've been trying to set up a two-stage bootloader for an FX3 device using the example code "Fx3BootAppGcc", but for the life of me I can't figure out ... Show More
Shafi
USB superspeed peripherals
Hi team, After flashing firmware in SPI flash through control center, how to make Cx3 auto reset to re-enumerate as UVC device without unplugging the ... Show More
Yamuna
USB superspeed peripherals
Hi all, This is regarding the Fx3S CPU sockets, FX3S supports one CY_U3P_CPU_SOCKET_PROD socket and one CY_U3P_CPU_SOCKET_CONS socket. In our applicat... Show More
rossi
USB superspeed peripherals
In my test thread when I call a function which contains CyU3PDmaChannelSetupRecvBuffer , the thread is not working after the function calling. (logs a... Show More
RaschTam
USB superspeed peripherals
Hi, I am strange behaviour with some of my address lines of my GPIF2 interface. My GPIF interface definition is: Asynchronous Master, 16 bit data bus ... Show More
TaOn_4865801
USB superspeed peripherals
We think that FX3 SDK is included a lot of function, API, RTOS, and sample firmware, but we do not know whether these files are open source or not.. Show More
JackLi
USB superspeed peripherals
Hello,    I have a problem when I use GPIF in 32bit  syncslave mode, my device is CYUSB3014.  And my GPIF setting is refering to AN65974  : 1) the Fla... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.