USB superspeed peripherals Forum Discussions
0x03 is trash?
2 bytes per pixel - > 640x480*2 = 614400 bytes (Frame)
Hello
How can I download the FPGA Configuration Utility tool(see the attachment) for CYUSB3014?.I want to Configure the xilinx FPGA over CYUSB3014.
Thanks.
Show LessHello,
Can the EZ-USB SX3 CYUSB3017-BZXI co-exist with PolarFire Microchip FPGA in the same electrical design although the SX3 Configuration Utility does not support the given FPGA?
Show Less
Open the EZUSBSUITE PC tool.
Could you please tell me, 1.suite installation and programming demo refer to that document .
2. GPIF II Designer installation and programming demos refer to that document.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%B6%85%E9%AB%98%E9%80%9FUSB%E5%A4%96%E8%AE%BE/FX3-1-3-3%E6%94%B9%E6%88%901-3-4/td-p/719450
Show LessHi,
We want to do a MIPI to USB 3.0 bridge for a IMX179 sensor.
We are interested only in images that are different from previosu one. So it would be very good to filter out (not send through USB 3.0 channel) those images that are "equal" (with some degree of flexibility) to the previos image. This way we use less the USB 3.0 pipe and save also host application capacity.
Is possible to make this with CX3?
Can we store the image in CX3 and then compare with the new one and compute some difference rank and decide whether to send or not the frame?
Thanks for your help
Show Less
Hi,
We are looking for a MIPI to USB 3.0 bridge to stream MJPEG video from an IMX179 sensor.
We need to support 3280x2464 @5FPS.
Can we use CX3 CYUSB3065 for that?
Show Less
Hi,
I'm currently trying to get the usb-uvc demos (USBVideoClass/UsbVideoClassBulk) from the sdk to work on the CYUSB3014. The issue i'm facing is that it works just fine in usb 2.0 but usb 3.0 is unresponsive (no uvc devices reporting).
i have found this post which seems to have been experiencing the same issue years ago:
The only issue is that their final answer is very vague, something about a frequency setting being wrong... But i can't seem to figure out what they're referring to or where the issue lies.
i've attached the unmodified demo i'm trying to get to work... any ideas?
In setting gpioClock how to set the member variables to achieve highest to lowest speed?:
fastClkDiv
slowClkDiv
simpleDiv
Hi ,
I need to test the bulk transfer on USB interface bulk-endpoints.For this I am going to use Streamer-Application comes with SDK .
But Application not detecting my device.
So What should I do ?
Show Less