USB Superspeed Peripherals

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
rossihwang
USB Superspeed Peripherals
Hardware host: tinker board 2s(rk3399),kernel 5.13 slave: sg130gs(1280*720, YUYV, 30fps) + fpga(spartan 6) + cyusb3014, isochronous mode Pro... Show More
EsPo_3827446
USB Superspeed Peripherals
I want to develop C++ application for fx3 bulk transfer IN? where I need to refer?  How much data (maximum data) can able to transfer in fx3 in sec? I... Show More
Turbo
USB Superspeed Peripherals
I have got a problem and need some help.I have designed a custom board refer to datasheet and a development board bought online.The board I desined co... Show More
dgrierms
USB Superspeed Peripherals
Hello, for our application we would like to use USB virtual com port to send/receive status messages with FX3s. My understanding is that I will need a... Show More
itayc
USB Superspeed Peripherals
Hi, I'm looking for reference code to run MIPI interface of the AR0144 Demo 3 Head board with FX3. Will appreciate any assistance. Thanks, Itay Cohen Show More
mcn
USB Superspeed Peripherals
I need to write synchronously to a DAC. No samples can be skipped. This requires multiple threads ping-ponging, just as it does on reading. However...... Show More
Ascs_4819156
USB Superspeed Peripherals
Dear Sir, I am using CYUSB3014 to develop a camera. Now it works normally at USB3.0 mode. But if I connect it to the USB2.0 port, it does not work wel... Show More
mcn
USB Superspeed Peripherals
Any additional details (or even a working example) would be helpful. Do we need to set DDR_MODE and DLE_PRESENT? Could we also DR_DATA at DDR?  Show More
Anonymous
USB Superspeed Peripherals
Dear All,                  We use Cypress FX3 machine vision products designed and requires the use of USB3 Vision agreements. I use the example provi... Show More
yxx0803
USB Superspeed Peripherals
你好,AN65974附带的FPGA代码--StreamIN的代码中,当填满缓冲区之后经过了一个时钟周期的 “stream_in_write_wr_delay”直接跳转到了“stream_in_idle”状态,在stream_in_idle状态下会去判断flaga_d的值,此时的flaga_d的值还... Show More