Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

Tomin
USB superspeed peripherals
Hello, I'm designing a custom PCB with FX3 to convert 8/14 bit DVP to UVC. Here I'm attaching the schematics for the same.With the help " Cypress FX3 ... Show More
jnagy
USB superspeed peripherals
In my GPIF state machine, I want to compare the 2bit address bus to a constant value and then transition state based on that comparison. Reading the d... Show More
jadhav_lokesh
USB superspeed peripherals
I've posted the below query on getting the Monochrome Camera working with FX3 and which is got resolved also. How-to-get-Monochrome-Camera-stream-working-on-FX3-using-AN75779... Show More
Nolan_Maverick
USB superspeed peripherals
We are trying to interface ov5640 with FX3  through Parallel Interface. We are able to perform I2c communication with Ov5640 using Fx3. We are trying ... Show More
Koki
USB superspeed peripherals
Hi Support, I have a technical question regarding the USB controller (CYUSB3014).A loopback function is required for USB communication evaluation,Is t... Show More
WiWo_1983446
USB superspeed peripherals
Our device uses the FX3 controller chip, running in Windows 10. The device always comes up with "Cypress FX3 USB BootLoader Device" in Device Manger a... Show More
liktenis
USB superspeed peripherals
Hello everyone, I am developing a USB3.0 peripheral using FX3. I am currently facing an issue where sometimes USB3.0 is recognized as USB2.0. Is there... Show More
Bambo
USB superspeed peripherals
Hi, I have trouble using the GPIF machine of my . Over the endpoint, some packets are lost, and some packets are not sent chronologically My system us... Show More
shaonWhite
USB superspeed peripherals
hello, we have developed a complete FX3 driver based on Cypress driver code. Now, we want to know whether our driver can be used on FX10(4014) periphe... Show More
jaewook
USB superspeed peripherals
Is there any reference code  about UAS?Currently I'm studying for USB msc with EZ USB FX3 board, but it's not easy to find any information about UAS.I... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.