USB superspeed peripherals Forum Discussions
I have to write a VHDL to interface my FX3 with an FPGA. I loaded the disc image AN65974 (slave fifo sync 2 bit) in the ram but i can't understand the endpoint addresses (flagA and FlagB). What they are? 00 - 01 - 10 - 11 ?
Show LessI am working with CX3 dev board for bring up ov5640 sensor.
Now, use the example, I can get YUV format image data, but I want to get raw10 format image data.
How to modify the code?
Show Lesshello everyone,
I am new to the cyusb suite for linux,i met a question that is how to load a firmware use the cyusb suite, i click the 'select file' button there just are .img file, In my PC Linux there exist a firmware (other gave me) but not a .img file.so i can't find it use the cyusb suite.so how can i load myself firmware ?advance for you help.
Show LessCan we connect CYUSB3KIT-003 to Aria10 using CYUSB3ACC-006?
Dear all,
Has anybody work with CX3 and OV13850 image sensor? or similar one.
Have you capture any image and bypass ir to a PC?
Thanks,
Iban.
Show LessI'm looking into using the Denebola RDK as a demonstration platform for a dual camera system. Is there any software issue that would prevent the use of two RDK's on the same Windows-10 computer?
Show LessHello,
I am merging slavefifo interface and gpiftostoarge fx3 firmware examples,
i am getting following errors,please find below and also attached firmware.
help me.
thank you
Show LessHi all,
We currently have a Windows project that uses the c++ library provided by the EZ-USB FX3 SDK (downloaded from: EZ-USB FX3 Software Development Kit | Cypress Semiconductor ). We are looking to cross-compile this project on mac. However, the sdk for mac does not seem to include this c++ api, only the c api is provided.
Is any way to obtain the mac binaries for the same c++ library? Is the source code perhaps available so we can build it ourselves? If not, I am open to suggestions to how to approach this problem.
Thanks for your help.
Show LessHi, I am using FX3S device for imaging and I am using Cypress FX3 SDK 1.3.3 version.
When I used examples from FX3 SDK which do not contain GPIF II interface(cyfxgpif2config.h file) it works fine.
However, when I used examples with GPIF II interface I get an error code of 997 in Control Center all of this type of examples.(UVC, U3V, Slave Fifo,Bulk Loop)t
What can be the reason for this issue in GPIF II designs? I have found GPIF Examples Not Working when Compiled with Libraries from FX3 SDK 1.3.3 - KBA223153 but it does not solve my problem.
Also when I tried 1.3.1 package I get an error code of 13 for ezUsbSuite which is shown below, if there is a solution for this, it is also be perfect.
Show LessHI,
I am using fx3s slavefifo example and gpifstorage example.
I am storing gpif p port data into the sd card (p port is producer and s port is consumer)and also recieving in the usb(p port is producer and u port is consumer),can i use same p port producer socket for both s and u port consumer sockets??
thank you...
Show Less