USB Superspeed Peripherals

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
EliW
USB Superspeed Peripherals
Hi,   I have FX3 and I use it for ISOC/Interrupt/BULK testing with the streamer app (add the app below) I wonder if there is an API for the app, Like ... Show More
Ash
USB Superspeed Peripherals
Hello all, I am working on FX3 while interfacing a camera sensor with it. I need to debug and as mentioned that there are some ways to do so using seg... Show More
Lee_sin
USB Superspeed Peripherals
你好我在做FPGA向FX3写数据的过程中遇到了一些问题想要明确一下: (缓冲区的大小设置为16kB,数据总线位宽为32位,水印值为6) 1、如果以16kB为单位写,这时候pktend_n信号是否可以一直处于高电平状态,并且我在control center中看到正确的数据。 2、以1024B为单位写,... Show More
louyuminghamn
USB Superspeed Peripherals
Hi,  There, We are using CYUSB3KIT-003 (the P/N of the chip is CYUSB3014) to design a camera. We need to send a leader and a trailer as single transfe... Show More
Myongho_Nov
USB Superspeed Peripherals
Hi. I'm  using CX3(CYUSB3065). When test using Stremer Program, the USB hub Operates normally. But Fail occurs when connecting directly to PC. How ca... Show More
jech_4828421
USB Superspeed Peripherals
Hi, I'm Jay. The question below has ended, so I'm posting the question again like this. https://community.infineon.com/t5/USB-Superspeed-Peripherals/UART-output-message-pending-problem/m-p/324177#M28797... Show More
LBence91
USB Superspeed Peripherals
Hello! I am trying develop an UVC application with the FX3 board(CYUSB3KIT). I am using as a base the AN75779 document and the UVC_AN75779 example pro... Show More
Subhash24
USB Superspeed Peripherals

Im working on a project about detecting black images can anyone tell me how to check it in Denebola Kit?

Thank you.

ElTa_4521156
USB Superspeed Peripherals
Hi, I am trying to read the serial number(SN) from the descriptor in a C++ code in Linux by libusb_get_string_descriptor_ascii. I read the SN first, t... Show More
Miquel
USB Superspeed Peripherals
Hi,   I am trying to program two different SPI nor flash memories using the Control Center. To do so, I want to use a GPIO from the FX3 to control a d... Show More