USB superspeed peripherals Forum Discussions
SDK Version is 1.3.4
I refer to KBA225748 to create a Cx3 project, but i can't find cyu3imagesensor.c - C file,
Steps to Setup up MIPI CSI Camera Solution with CX... - Infineon Developer Community
i only can find cyu3imagesensor.h file, this Header file is loacted in SDK lib folder.
How to generate or get cyu3imagesensor.c - C file.
Show LessIs FX3 compatible with Android Open Source Platform (AOSP)?
Infineon has specific support for Android with their USB-Serial Bridge Controllers. Reference USB-Serial SDK @ https://www.infineon.com/cms/en/design-support/tools/sdk/usb-controllers-sdk/usb-serial-software-development-kit/
No similar support for Android appears for FX3 SDK @ https://www.infineon.com/cms/en/design-support/tools/sdk/usb-controllers-sdk/ez-usb-fx3-software-development-kit/
An old post on Infineon’s Community from 2017 notes Infineon’s FX3 does not provide any android specific drivers FX3 Cy3014 support android driver? - Infineon Developer Community
Greg
Show LessPlease update the link to the Ap Notes @ https://www.infineon.com/cms/en/design-support/software/code-examples/usb-controllers-code-examples/usb-super-speed-code-examples/
The links under the AN-PDF column return an error.
Service Unavailable - DNS failure
The server is temporarily unable to service your request. Please try again later.
Reference #11.a660dc17.1692023977.1a36e20
Note: The links under the AN-Code column appear to work by downloading the zip file of the source code
Greg
Show Less
Hello Infineon! This is getting long sorry:
To summarize the issue, there is no SIB boot method in boot_fw.
The reason I need to do this is to encrypt the main firmware loaded onto the drive. In the future we might look into getting FIPS 140-3 lvl 2 or 3 with FX3s.
Q 1. Is there a method to use normal firmware to perform a jump to another firmware operation like what is provided in boot_fw?
Q 2. Does the posisitions set in the ld files need to be retained after a different firmware starts?
Q 3. Can I get a package with the tools needed to compile boot_fw to add SIB support into it? I won't do this if Question 2 works.
I'm still not clear about the purpose of the 32kb's at the end of Sys_mem, it was brought up in this forum post I made earlier, I don't think I was been clear: https://community.infineon.com/t5/USB-superspeed-peripherals/Clarity-on-second-stage-boot-area-purpose/m-p/441219#M34194
To rephrase the question: Given this scenario:
2 firmwares: Boot loader and main firmware
1. Boot loader firmware with concatenated/stored firmware runs/starts from the last 32KB's in Sys_mem
2. Loads main firmware into start address (0x40000000 I think maybe 0x40003000, from SPI or iC2 storage)
3. Jump FX3 to start of main firmware address and starts main firmware
At this point, as the main firmware is now running, why does main firmware need to retain that 32kb's in Sysmem? Can it jump back to this firmware or is there a checksum/tamper protection reason? It seems like it can now be overwritten and used safely.
My current problem is that we have ONLY SIB drive for firmware on an eMMC chip, and boot_fw does not have a method for handling this. The 2 ideas I'm about to try to play around with is:
1. Rewriting boot_fw's cyfx3.ld's memory position from: 0x40078000 to the position used for the start of "Data Area" of the main firmware set in fx3.ld (PLEASE CORRECT ME if this is not how firmware is loaded up into FX3's RAM, I am basing this from the reply in previous post linked above) This is approximately the half way point of the 512kb's RAM on fx3s.
-This way I can make the main firmware as a large array within boot loader firmware (Memory location Data in boot's fx3.ld file modified accordingly), I should also be able to use a compression method on it too reducing the actual firmware file size stored.
-For any future firmware updates, I will just switch between boot options 0 and 1 (NOTE SIB drive is split into 4 partition: 0 and 1 boot, 2 data, 3 data) so modifying/dynamicly loading from SIB should not be an issue.
2. Recompile boot_fw with SIB source from normal firmware. I haven't had luck with this yet, to go down this route, I would greatly appreciate a package of tools or links to the correct versions of them such as Cygwin etc. used instead of just the pdf: https://community.infineon.com/gfawx74859/attachments/gfawx74859/usb-superspeed-peripherals/5750/1/FX3FirmwareSourceUserGuide.pdf)
-Please note I had a similar hard time compiling the boot firmware loader for fx3s with visual studio, that required some obscure version of the DDK for windows 8.1 or something like that.... Newer/older versions didn't work
-This way I can use the boot_fw with SIB (card manager) and the recommended approach can be followed. I am more then happy to share the resulting source code for boot_fw with SIB too.
Regards!
Fujimi
Show LessWe are using CYUSB3.sys for an application with many usb devices attached. Is there a limitation to the number of devices which this driver can control? We had a legacy driver (ezusb.sys) that had an internal limit of 32. I've looked at the documentation and headers and couldn't identify such a limit.
Thanks for any help / insight
Show LessDear Team,
I need to use a GPIO for a reset control for my image sensor and other deices. for that I'm trying to add simple on GPIO control to my CSI generated code but when I add these following lines my device is no longer enumerating as a UVC device or any other device.
I have attached the project file.
Hi,
I have troubles using simultaneously the GPIF machine and the Fx3 firmware part.
My application is a video streaming device.
My Fx3 system uses 3 endpoints, 2 for command exchange with the host, and 1 for data streaming.
I also actively use the available UART, using a manual DMA IN and manual DMA OUT.
See below the configuration of my endpoints :
Command endpoints configuration :
CyU3PMemSet ((uint8_t *)&epCfg, 0, sizeof (epCfg));
epCfg.enable = CyTrue;
epCfg.epType = CY_U3P_USB_EP_BULK;
epCfg.burstLen = 1;
epCfg.streams = 0;
epCfg.pcktSize = size;
/* DCI Out EP configuration */
stat = CyU3PSetEpConfig(CY_FX_EP_DCI_CMD, &epCfg);
if (stat != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "CyU3PSetEpConfig failed for CY_FX_EP_DCI_CMD, Error code = %x\n", stat);
CyFxAppErrorHandler (stat);
}
/* DCI In EP configuration */
stat = CyU3PSetEpConfig(CY_FX_EP_DCI_RSP, &epCfg);
if (stat != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "CyU3PSetEpConfig failed for CY_FX_EP_DCI_RSP, Error code = %x\n", stat);
CyFxAppErrorHandler (stat);
}
Data endpoint configuration:
/* Configure the video streaming endpoint. */
memset(& endPointConfig, 0, sizeof(endPointConfig));
endPointConfig.enable = 1;
endPointConfig.epType = CY_U3P_USB_EP_BULK;
endPointConfig.pcktSize = CY_FX_EP_BULK_VIDEO_PKT_SIZE; //1024
endPointConfig.burstLen = CY_FX_EP_BULK_VIDEO_PKTS_COUNT; // 16
endPointConfig.streams = 0;
apiRetStatus = CyU3PSetEpConfig (CY_FX_EP_DSI_STREAM, &endPointConfig);
if (apiRetStatus != CY_U3P_SUCCESS)
{
sendUARTDebugMessage("Error : CyU3PSetEpConfig (CY_FX_EP_DSI_STREAM, &endPointConfig)");
return apiRetStatus;
/* Error Handling */
// CyFxAppErrorHandler ("CyU3PSetEpConfig (CY_FX_EP_BULK_VIDEO", apiRetStatus);
}
Now the thing is that when I keep my GPIF shut down, I have no command lost on the Fx3 Firmware side.
When I activate my GPIF machine, but have no data streaming, I have no command lost on the Fx3 Firmware side either.
But when I activate my GPIF machine, and have data streaming, I have every commands lost on the Fx3 Firmware side.
This prevents me from shutting down the streaming, hence I can't recover from streaming.
See below my wireshark capture of a video streaming
No data streaming example, Fx3 firmware can answer everything :
Below, the firmware also streams data (Blocks in tha capture), but Fx3 firmware fails to answer properly, even though it usually can.
Highlighted are the same commands sequence wise.
About the data flow I use in the Fx3 firmware, I use the firmware infinite loop to wait for commands, and answer as soon as possible.
In the case of a command that is long to answer, I send a pending acknowledge packet, before sending the final answer.
In that case, I call CyU3PThreadSleep() to wait for the needed time, before resuming my activity in the infinite loop.
The data flow is summarized below. (CPUProd and UARTProd are the DMA channels I use for UART communication)
It seems that the infinite loop fails to work when the GPIF is also working. According to my tests and traces, it fails somewhere between step 5 and step 6, close to the CyU3PThreadSleep() call.
Do you have any suggestion ?
Thanks !
Bambo
Show LessHi,
I would like to use FX3 controller to directly connect the parallel LVDS output from a 14-bit dual channel ADC with 250MSPS. From the datasheet of the device, it is clear that I can connect ADC output to the pins of GPIFII interface, and it can connect that to USB port. My questions are:
1) Can I connect dual channel ADC to FX3 controller? I am planning to use analog devices AD9643BCPZ-250 ADC for my application. Is this compatible to FX3? Please find datasheet of ADC below.
2) My application with ADC is to convert the IQ baseband to digital. Can I use FX3 for such kind of applications? Or FX3 is dedicated only for video signals?
3) I would like to store the data on fast memory on the device itself. Is it possible with FX3 controllers?
Thank you in advance.
Regards
https://www.analog.com/media/en/technical-documentation/data-sheets/AD9643.pdf |