Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

KeWa_2323766
USB superspeed peripherals
In my application, I2C flash memory will be used for FX3 firmware image. At the same time, I have I2C interfaced temperature sensor that FX3 need to i... Show More
MaBa_1857101
USB superspeed peripherals
HI,Is it possible to change defult state of the GPIO pins(in bootloader mode)?During bootloader mode, GPIO 51 held in LOW. is it possible to change to... Show More
ScGr_289066
USB superspeed peripherals
Hi,I have successfully streamed RAW10 from the OV5647 sensor and thought it would be an easy matter to reduce that to RAW8.  It has not been.  I refer... Show More
UnHa_3846631
USB superspeed peripherals
Hello,CY4500 is avaliable to measure current or voltage of USB 3.0 Device which not applyed USB PD controller?? Show More
hahac_299066
USB superspeed peripherals
hi,I have some problem when I use "CyUSB.dll", when I run my app, the first run it, everything is ok, but for the second time, I got a message, I don'... Show More
qiko_3575871
USB superspeed peripherals
Hello every. Could somebody give me some advice?I have an android device and a Cypress device. I want to connect them. And transfer data between them.... Show More
veRN_2322216
USB superspeed peripherals
hello,         I am working on fx3s to fetch data from fpga to host Pc. while doing this i want to fetch some data like firmware version and hardware ... Show More
Anonymous
USB superspeed peripherals
I've changed "USBVideoClass" example from MJPEG to YUV(from subtype : VS_FORMAT_MJPEG to Subtype : uncompressed format)The descriptors are originally ... Show More
DaBo_288066
USB superspeed peripherals
Hello,sorry but I have to create a new discussion since my previous post (USB-IF Link Layer Test failed ) has been prematurely locked...I tried to com... Show More
doch_3739346
USB superspeed peripherals
Hi,RD_START is the START State for read command.SRAM_READ_COMMAND, CyU3PGpifSMSwitch start state changed to RD_START.Linux application read from endpo... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.