Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB superspeed peripherals Forum Discussions

gean_3054931
USB superspeed peripherals
Hello,I am using JLINK BASE with cypress EZ USB sdk .I am getting ERROR: Bad JTAG communication: Write to IR: Expected 0x1, got 0x7 (TAP Command : 15)... Show More
Peya_4162826
USB superspeed peripherals

I want to get the system tick in millisecond, which function can get it?

rolic_4206696
USB superspeed peripherals
Hi:     I want to use cdc virtual uart as a debug uart, but PC uart tool can not print  anything.can you help me? Show More
Peya_4162826
USB superspeed peripherals
when debug message output is OK, then use CyU3PTimerCreate to create one timer, use CyU3PDebugPrint in timer call back function, It can not print mess... Show More
MaMa_4034336
USB superspeed peripherals
Hello,I'm trying to send raw Image data with my CYUSB3KIT-003 to my PC. However currently it looks like my program to send the data is to slow (I get ... Show More
SaGi_4116301
USB superspeed peripherals
Hello,I am using the EZ USB FX3 board to build an interface to an external device that requires an approx. 100MHz clock and puts out a serial 100MHz s... Show More
ElRu_4198366
USB superspeed peripherals
Hi Cypress,We using CYUSB3KIT-003 development kit to test the "cyfxisosrcsink" firmware project, and attachd we encounter abnormal data streaming whil... Show More
yiwa_4244806
USB superspeed peripherals
Hi there,When I was reviewing source code for FX3 U3V device, I found a question as below:the function source code is:=== uint32_t *uniqueIDreg = (uin... Show More
Peya_4162826
USB superspeed peripherals
Import project “C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\msc_examples\cyfxmscdemo”, then select build project, appear following erro... Show More
yvjec_3905651
USB superspeed peripherals
Hey there,Since more than ten years were using a CY7C68013 USB without any big problems. However, we recently noticed customer increasing complaining ... Show More
Forum Information

USB superspeed peripherals

Discussion forum regarding USB superspeed peripherals topics.