USB superspeed peripherals Forum Discussions
text.format{('custom.tabs.no.results')}
Dear all,
This thread refers to debugging the DENEBOLA CX3 evaluation board using SEgger J-Link when using Linux (Ubuntu) Platform.
I follow both EzUsbSuite_UG.pdf and FX3_SDK_Linux_Support.pdf document sfor that matter.
From eclipse I tried to debug the sample application that demonstrates data transfer from the FX3 GPIF port to the USB port with no success.
It looks like the debugger is stuck - cannot step over \ step into.
please see console log below:
./JLinkGDBServer -device ARM9
SEGGER J-Link GDB Server V6.54c Command Line Version
JLinkARM.dll V6.54c (DLL compiled Nov 7 2019 17:05:41)
Command line: -device ARM9
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: yes
Generate logfile: off
Verify download: off
Init regs on start: off
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: ARM9
Target interface: JTAG
Target interface speed: 4000kHz
Target endian: little
Connecting to J-Link...
J-Link is connected.
Firmware: J-Link V10 compiled Oct 22 2019 16:28:15
Hardware: V10.10
S/N: 50119080
Feature(s): GDB
Checking target voltage...
Target voltage: 3.32 V
Listening on TCP/IP port 2331
Connecting to target...
J-Link found 1 JTAG device, Total IRLen = 4
JTAG ID: 0x07926069 (ARM9)
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0xF0000048 (Data = 0xEAFFFFFE)
Received monitor command: speed 1000
Target interface speed set to 1000 kHz
Received monitor command: clrbp
Received monitor command: reset
WARNING: PC of target system has unexpected value of 0xF00002A8 after reset.
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x00000000)
Received monitor command: regs
PC = 00000000, CPSR = 000000D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000
R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000
USR: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000
R13=00000000, R14=00000000
FIQ: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000
R13=00000000, R14=00000000, SPSR=00000010
SVC: R13=00000000, R14=00000000, SPSR=00000010
ABT: R13=00000000, R14=00000000, SPSR=00000010
IRQ: R13=00000000, R14=00000000, SPSR=00000010
UND: R13=00000000, R14=00000000, SPSR=00000010
Reading all registers
Received monitor command: speed auto
Select auto target interface speed (7827 kHz)
Received monitor command: flash breakpoints 1
Flash breakpoints enabled
Received monitor command: semihosting enable
Semi-hosting enabled (SVC Addr = 0x08)
Received monitor command: semihosting IOClient 1
Semihosting I/O set to TELNET Client
Downloading 9512 bytes @ address 0x00000100
Downloading 11416 bytes @ address 0x40003000
Downloading 16 bytes @ address 0x40005C98
Downloading 92 bytes @ address 0x40005CA8
Downloading 232 bytes @ address 0x40005D04
Downloading 212 bytes @ address 0x40005DEC
Downloading 68 bytes @ address 0x40005EC0
Downloading 536 bytes @ address 0x40005F04
Downloading 80 bytes @ address 0x4000611C
Downloading 132 bytes @ address 0x4000616C
Downloading 84 bytes @ address 0x400061F0
Downloading 752 bytes @ address 0x40006244
Downloading 152 bytes @ address 0x40006534
Downloading 620 bytes @ address 0x400065CC
Downloading 1016 bytes @ address 0x40006838
Downloading 180 bytes @ address 0x40006C30
Downloading 212 bytes @ address 0x40006CE4
Downloading 456 bytes @ address 0x40006DB8
Downloading 848 bytes @ address 0x40006F80
Downloading 820 bytes @ address 0x400072D0
Downloading 288 bytes @ address 0x40007604
Downloading 140 bytes @ address 0x40007724
Downloading 248 bytes @ address 0x400077B0
Downloading 100 bytes @ address 0x400078A8
Downloading 436 bytes @ address 0x4000790C
Downloading 220 bytes @ address 0x40007AC0
Downloading 416 bytes @ address 0x40007B9C
Downloading 492 bytes @ address 0x40007D3C
Downloading 544 bytes @ address 0x40007F28
Downloading 236 bytes @ address 0x40008148
Downloading 304 bytes @ address 0x40008234
Downloading 420 bytes @ address 0x40008364
Downloading 268 bytes @ address 0x40008508
Downloading 276 bytes @ address 0x40008614
Downloading 240 bytes @ address 0x40008728
Downloading 52 bytes @ address 0x40008818
Downloading 412 bytes @ address 0x4000884C
Downloading 128 bytes @ address 0x400089E8
Downloading 16 bytes @ address 0x40008A68
Downloading 592 bytes @ address 0x40008A78
Downloading 248 bytes @ address 0x40008CC8
Downloading 696 bytes @ address 0x40008DC0
Downloading 108 bytes @ address 0x40009078
Downloading 152 bytes @ address 0x400090E4
Downloading 336 bytes @ address 0x4000917C
Downloading 152 bytes @ address 0x400092CC
Downloading 1168 bytes @ address 0x40009364
Downloading 128 bytes @ address 0x400097F8
Downloading 44 bytes @ address 0x40009878
Downloading 244 bytes @ address 0x400098A4
Downloading 208 bytes @ address 0x40009998
Downloading 156 bytes @ address 0x40009A68
Downloading 64 bytes @ address 0x40009B04
Downloading 120 bytes @ address 0x40009B44
Downloading 192 bytes @ address 0x40009BC0
Downloading 960 bytes @ address 0x40009C80
Downloading 1536 bytes @ address 0x4000A040
Downloading 1516 bytes @ address 0x4000A640
Downloading 1684 bytes @ address 0x4000AC2C
Downloading 80 bytes @ address 0x4000B2C0
Downloading 248 bytes @ address 0x4000B310
Downloading 64 bytes @ address 0x4000B408
Downloading 412 bytes @ address 0x4000B448
Downloading 276 bytes @ address 0x4000B5E4
Downloading 60 bytes @ address 0x4000B6F8
Downloading 60 bytes @ address 0x4000B734
Downloading 100 bytes @ address 0x4000B770
Downloading 112 bytes @ address 0x4000B7D4
Downloading 352 bytes @ address 0x4000B848
Downloading 160 bytes @ address 0x4000B9A8
Downloading 224 bytes @ address 0x4000BA48
Downloading 16 bytes @ address 0x4000BB28
Downloading 104 bytes @ address 0x4000BB38
Downloading 156 bytes @ address 0x4000BBA0
Downloading 256 bytes @ address 0x4000BC3C
Downloading 164 bytes @ address 0x4000BD3C
Downloading 144 bytes @ address 0x4000BDE0
Downloading 628 bytes @ address 0x4000BE70
Downloading 340 bytes @ address 0x4000C0E4
Downloading 56 bytes @ address 0x4000C238
Downloading 132 bytes @ address 0x4000C270
Downloading 160 bytes @ address 0x4000C2F8
Downloading 40 bytes @ address 0x4000C398
Downloading 416 bytes @ address 0x4000C3C0
Downloading 296 bytes @ address 0x4000C560
Downloading 80 bytes @ address 0x4000C688
Downloading 304 bytes @ address 0x4000C6D8
Downloading 216 bytes @ address 0x4000C808
Downloading 132 bytes @ address 0x4000C8E0
Downloading 12 bytes @ address 0x4000C964
Downloading 12 bytes @ address 0x4000C970
Downloading 16 bytes @ address 0x4000C97C
Downloading 16 bytes @ address 0x4000C98C
Downloading 20 bytes @ address 0x4000C99C
Downloading 16 bytes @ address 0x4000C9B0
Downloading 12 bytes @ address 0x4000C9C0
Downloading 20 bytes @ address 0x4000C9CC
Downloading 60 bytes @ address 0x4000C9E0
Downloading 40 bytes @ address 0x4000CA1C
Downloading 124 bytes @ address 0x4000CA44
Downloading 336 bytes @ address 0x4000CAC0
Downloading 356 bytes @ address 0x4000CC10
Downloading 80 bytes @ address 0x4000CD74
Downloading 688 bytes @ address 0x4000CDC4
Downloading 388 bytes @ address 0x4000D074
Downloading 96 bytes @ address 0x4000D1F8
Downloading 160 bytes @ address 0x4000D258
Downloading 224 bytes @ address 0x4000D2F8
Downloading 224 bytes @ address 0x4000D3D8
Downloading 72 bytes @ address 0x4000D4B8
Downloading 172 bytes @ address 0x4000D500
Downloading 116 bytes @ address 0x4000D5AC
Downloading 212 bytes @ address 0x4000D620
Downloading 356 bytes @ address 0x4000D6F4
Downloading 232 bytes @ address 0x4000D858
Downloading 176 bytes @ address 0x4000D940
Downloading 16 bytes @ address 0x4000D9F0
Downloading 36 bytes @ address 0x4000DA00
Downloading 120 bytes @ address 0x4000DA28
Downloading 4 bytes @ address 0x4000DAA0
Downloading 584 bytes @ address 0x4000DAA4
Downloading 16 bytes @ address 0x4000DCEC
Downloading 204 bytes @ address 0x4000DCFC
Downloading 192 bytes @ address 0x4000DDC8
Downloading 16 bytes @ address 0x4000DE88
Downloading 1360 bytes @ address 0x4000DE98
Downloading 132 bytes @ address 0x4000E3E8
Downloading 456 bytes @ address 0x4000E46C
Downloading 344 bytes @ address 0x4000E634
Downloading 248 bytes @ address 0x4000E78C
Downloading 372 bytes @ address 0x4000E884
Downloading 148 bytes @ address 0x4000E9F8
Downloading 188 bytes @ address 0x4000EA8C
Downloading 440 bytes @ address 0x4000EB48
Downloading 180 bytes @ address 0x4000ED00
Downloading 300 bytes @ address 0x4000EDB4
Downloading 4 bytes @ address 0x4000EEE0
Downloading 16 bytes @ address 0x4000EEE4
Downloading 16 bytes @ address 0x4000EEF4
Downloading 76 bytes @ address 0x4000EF04
Downloading 104 bytes @ address 0x4000EF50
Downloading 108 bytes @ address 0x4000EFB8
Downloading 124 bytes @ address 0x4000F024
Downloading 180 bytes @ address 0x4000F0A0
Downloading 588 bytes @ address 0x4000F154
Downloading 892 bytes @ address 0x4000F3A0
Downloading 12 bytes @ address 0x4000F71C
Downloading 4 bytes @ address 0x4000F728
Downloading 800 bytes @ address 0x4000F72C
Downloading 212 bytes @ address 0x4000FA4C
Downloading 120 bytes @ address 0x4000FB20
Downloading 592 bytes @ address 0x4000FB98
Downloading 244 bytes @ address 0x4000FDE8
Downloading 456 bytes @ address 0x4000FEDC
Downloading 436 bytes @ address 0x400100A4
Downloading 168 bytes @ address 0x40010258
Downloading 340 bytes @ address 0x40010300
Downloading 1008 bytes @ address 0x40010454
Downloading 940 bytes @ address 0x40010844
Downloading 128 bytes @ address 0x40010BF0
Downloading 128 bytes @ address 0x40010C70
Downloading 120 bytes @ address 0x40010CF0
Downloading 440 bytes @ address 0x40010D68
Downloading 528 bytes @ address 0x40010F20
Downloading 640 bytes @ address 0x40011130
Downloading 224 bytes @ address 0x400113B0
Downloading 60 bytes @ address 0x40011490
Downloading 160 bytes @ address 0x400114CC
Downloading 160 bytes @ address 0x4001156C
Downloading 1272 bytes @ address 0x4001160C
Downloading 316 bytes @ address 0x40011B04
Downloading 1572 bytes @ address 0x40011C40
Downloading 196 bytes @ address 0x40012264
Downloading 164 bytes @ address 0x40012328
Downloading 144 bytes @ address 0x400123D0
Downloading 360 bytes @ address 0x40012460
Downloading 132 bytes @ address 0x400125C8
Downloading 608 bytes @ address 0x4001264C
Downloading 48 bytes @ address 0x400128B0
Downloading 544 bytes @ address 0x400128E0
Downloading 696 bytes @ address 0x40012B00
Downloading 184 bytes @ address 0x40012DB8
Downloading 24 bytes @ address 0x40012E70
Downloading 280 bytes @ address 0x40012E88
Downloading 1204 bytes @ address 0x40012FA0
Downloading 248 bytes @ address 0x40013454
Downloading 304 bytes @ address 0x4001354C
Downloading 96 bytes @ address 0x40013680
Downloading 540 bytes @ address 0x400136E0
Downloading 84 bytes @ address 0x400138FC
Downloading 16 bytes @ address 0x40013950
Downloading 96 bytes @ address 0x40013960
Downloading 376 bytes @ address 0x400139C0
Downloading 80 bytes @ address 0x40013B38
Downloading 568 bytes @ address 0x40013B88
Downloading 480 bytes @ address 0x40013DC0
Downloading 424 bytes @ address 0x40013FA0
Downloading 528 bytes @ address 0x40014148
Downloading 2128 bytes @ address 0x40014358
Downloading 80 bytes @ address 0x40014BA8
Downloading 304 bytes @ address 0x40014BF8
Downloading 824 bytes @ address 0x40014D28
Downloading 260 bytes @ address 0x40015060
Downloading 92 bytes @ address 0x40015164
Downloading 32 bytes @ address 0x400151C0
Downloading 104 bytes @ address 0x400151E0
Downloading 40 bytes @ address 0x40015248
Downloading 32 bytes @ address 0x40015270
Downloading 276 bytes @ address 0x40015290
Downloading 12 bytes @ address 0x400153A4
Downloading 16 bytes @ address 0x400153B0
Downloading 20 bytes @ address 0x400153C0
Downloading 20 bytes @ address 0x400153D4
Downloading 12 bytes @ address 0x400153E8
Downloading 64 bytes @ address 0x400153F8
Downloading 64 bytes @ address 0x40015438
Downloading 24 bytes @ address 0x40015478
Downloading 404 bytes @ address 0x40015490
Downloading 16 bytes @ address 0x40015624
Downloading 16 bytes @ address 0x40015634
Downloading 16 bytes @ address 0x40015644
Downloading 16 bytes @ address 0x40015654
Downloading 628 bytes @ address 0x40015664
Downloading 168 bytes @ address 0x400158D8
Downloading 116 bytes @ address 0x40015980
Downloading 40 bytes @ address 0x400159F4
Downloading 40 bytes @ address 0x40015A1C
Downloading 40 bytes @ address 0x40015A44
Downloading 40 bytes @ address 0x40015A6C
Downloading 40 bytes @ address 0x40015A94
Downloading 40 bytes @ address 0x40015ABC
Downloading 40 bytes @ address 0x40015AE4
Downloading 48 bytes @ address 0x40015B0C
Downloading 104 bytes @ address 0x40015B3C
Downloading 20 bytes @ address 0x40015BA4
Downloading 84 bytes @ address 0x40015BB8
Downloading 48 bytes @ address 0x40015C0C
Downloading 24 bytes @ address 0x40015C3C
Downloading 24 bytes @ address 0x40015C54
Downloading 68 bytes @ address 0x40015C6C
Downloading 48 bytes @ address 0x40015CB0
Downloading 44 bytes @ address 0x40015CE0
Downloading 128 bytes @ address 0x40015D0C
Downloading 148 bytes @ address 0x40015D8C
Downloading 184 bytes @ address 0x40015E20
Downloading 88 bytes @ address 0x40015ED8
Downloading 112 bytes @ address 0x40015F30
Downloading 100 bytes @ address 0x40015FA0
Downloading 264 bytes @ address 0x40016004
Downloading 376 bytes @ address 0x4001610C
Downloading 132 bytes @ address 0x40016284
Downloading 120 bytes @ address 0x40016308
Downloading 276 bytes @ address 0x40016380
Downloading 256 bytes @ address 0x40016494
Downloading 452 bytes @ address 0x40016594
Downloading 1540 bytes @ address 0x40016758
Downloading 324 bytes @ address 0x40016D5C
Downloading 236 bytes @ address 0x40016EA0
Downloading 580 bytes @ address 0x40016F8C
Downloading 80 bytes @ address 0x400171D0
Downloading 272 bytes @ address 0x40017220
Downloading 400 bytes @ address 0x40017330
Downloading 128 bytes @ address 0x400174C0
Downloading 140 bytes @ address 0x40017540
Downloading 320 bytes @ address 0x400175CC
Downloading 128 bytes @ address 0x4001770C
Downloading 192 bytes @ address 0x4001778C
Downloading 104 bytes @ address 0x4001784C
Downloading 376 bytes @ address 0x400178B4
Downloading 128 bytes @ address 0x40017A2C
Downloading 212 bytes @ address 0x40017AAC
Downloading 160 bytes @ address 0x40017B80
Downloading 440 bytes @ address 0x40017C20
Downloading 160 bytes @ address 0x40017DD8
Downloading 160 bytes @ address 0x40017E78
Downloading 160 bytes @ address 0x40017F18
Downloading 612 bytes @ address 0x40017FB8
Downloading 116 bytes @ address 0x4001821C
Downloading 160 bytes @ address 0x40018290
Downloading 52 bytes @ address 0x40018330
Downloading 64 bytes @ address 0x40018364
Downloading 64 bytes @ address 0x400183A4
Downloading 136 bytes @ address 0x400183E4
Downloading 456 bytes @ address 0x4001846C
Downloading 64 bytes @ address 0x40018634
Downloading 712 bytes @ address 0x40018674
Downloading 208 bytes @ address 0x4001893C
Downloading 600 bytes @ address 0x40018A0C
Downloading 588 bytes @ address 0x40018C64
Downloading 440 bytes @ address 0x40018EB0
Downloading 712 bytes @ address 0x40019068
Downloading 460 bytes @ address 0x40019330
Downloading 588 bytes @ address 0x400194FC
Downloading 720 bytes @ address 0x40019748
Downloading 1512 bytes @ address 0x40019A18
Downloading 168 bytes @ address 0x4001A000
Downloading 472 bytes @ address 0x4001A0A8
Downloading 732 bytes @ address 0x4001A280
Downloading 756 bytes @ address 0x4001A55C
Downloading 136 bytes @ address 0x4001A850
Downloading 1236 bytes @ address 0x4001A8D8
Downloading 524 bytes @ address 0x4001ADAC
Downloading 956 bytes @ address 0x4001AFB8
Downloading 1120 bytes @ address 0x4001B374
Downloading 940 bytes @ address 0x4001B7D4
Downloading 828 bytes @ address 0x4001BB80
Downloading 424 bytes @ address 0x4001BEBC
Downloading 416 bytes @ address 0x4001C064
Downloading 752 bytes @ address 0x4001C204
Downloading 464 bytes @ address 0x4001C4F4
Downloading 156 bytes @ address 0x4001C6C4
Downloading 212 bytes @ address 0x4001C760
Downloading 76 bytes @ address 0x4001C834
Downloading 176 bytes @ address 0x4001C880
Downloading 968 bytes @ address 0x4001C930
Downloading 360 bytes @ address 0x4001CCF8
Downloading 108 bytes @ address 0x4001CE60
Downloading 320 bytes @ address 0x4001CECC
Downloading 300 bytes @ address 0x4001D00C
Downloading 508 bytes @ address 0x4001D138
Downloading 628 bytes @ address 0x4001D334
Downloading 60 bytes @ address 0x4001D5A8
Downloading 164 bytes @ address 0x4001D5E4
Downloading 428 bytes @ address 0x4001D688
Downloading 148 bytes @ address 0x4001D834
Downloading 208 bytes @ address 0x4001D8C8
Downloading 208 bytes @ address 0x4001D998
Downloading 628 bytes @ address 0x4001DA68
Downloading 232 bytes @ address 0x4001DCDC
Downloading 1048 bytes @ address 0x40030000
Writing register (PC = 0x4000bcf8)
Read 4 bytes @ address 0x4000BCF8 (Data = 0xE59F1034)
Read 2 bytes @ address 0x40003F1A (Data = 0x2300)
Read 2 bytes @ address 0x40003F4E (Data = 0x6BFB)
Read 2 bytes @ address 0x40003F1A (Data = 0x2300)
Read 2 bytes @ address 0x40003F1A (Data = 0x2300)
Read 2 bytes @ address 0x40003F1A (Data = 0x2300)
Received monitor command: clrbp
Received monitor command: reset
WARNING: PC of target system has unexpected value of 0xF001C144 after reset.
Resetting target
Received monitor command: halt
Halting target CPU...
...Target halted (PC = 0x00000000)
Received monitor command: regs
PC = 00000000, CPSR = 000000D3 (SVC mode, ARM FIQ dis. IRQ dis.)
R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000
R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000
USR: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000
R13=00000000, R14=00000000
FIQ: R8 =00000000, R9 =00000000, R10=00000000, R11 =00000000, R12 =00000000
R13=00000000, R14=00000000, SPSR=00000010
SVC: R13=00000000, R14=00000000, SPSR=00000010
ABT: R13=00000000, R14=00000000, SPSR=00000010
IRQ: R13=00000000, R14=00000000, SPSR=00000010
UND: R13=00000000, R14=00000000, SPSR=00000010
Reading all registers
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0x17B514D7)
Setting breakpoint @ address 0x40003F1A, Size = 2, BPHandle = 0x0002
Setting breakpoint @ address 0x40003F4E, Size = 2, BPHandle = 0x0003
Starting target CPU...
Please advise,
Show LessI followed the CyUSB Suite for Linux document on Ubuntu 14.04, installed Qt4 and libusb 1.0, built the cyusb library. Tried to program the FX3 with cyfxbulksrcsink, write data at end point 0x01 and it worked fine. But when try to read from 0x81, it suppose to return some constant data, but I always read back nothing.
This works on Windows. Do you anything special needs to be done for this to work?
Thanks,
Frank.
Show Less请问下Cypress有USB3.0和PCIE互转的方案嘛?有的话请推荐下,谢谢!
Dear members
I will use tCYUSB3610 between AP Chip set USB Port and CYSYB3610.
Q1) I can't assign D+/D- from AP to CYUSB3610.
Can I use CYUSB 3601 to converter from USB to gigabit ethernet if CYUSB3610 DP/DM Pin is no connection Pin?
Q2) Becaus of board don't use USB Connector , VBUS will be supplied to 5V using LDO.
Is there no problem?
I am waiting opinios.
Thanks
Show LessDear all,
For a new project in the company i work for, I would like to check out the option to use Cypress CX3 SoC.
One of the requirements of the project is to stream a video from the CX3 via USB UVC class to a host PC @ 30fps.
In addition, there is a need to add a timestamp for each video frame by utilizing the PTS field (Presentation Time Stamp) of the UVC payload header.
Is there a way to support this requirement without compromising system performance (i.e. stream video frame @ 30fps)
Please advise,
Nissim.
Show LessHello,
I am implementing USB-C using the PIUSB302 multiplexer as described in KBA218460. Unfortunately there are references to two symbols: U3_EVENT and U3_TRUE which are not defined. Can you provide definitions for these symbols?
Thanks,
Scott
Show LessHello
I have done to create a Configuration with Basic Settings with CX3 Image Sensor Configuration in the CX3RDK_OV5640 project of e-ConStystem.
The MIPI project(New sensor project) build passes, but there is a red mark as attached. Q1) Could you please tell me the reason on this red circle?
Q2-1)Also, where should the files generated by MIPI configuration be linked in the OVRDK_OV560 project? Q2-2) Or what steps are required to implement the MIPI project itself under the CX3RDK_OV560 project?
Best Regards
Arai
Show LessI'm using USB2.0 port. Resolution of a camera is VGA.
Hello!
I work on Slave FIFO + UART firmware based on Cypress examples.
I ran into very strange bug - I get CyFxUSBUARTDmaCallback() (which is callback for DMA_MANUAL channel between uart producer socket and usb consumer socket) call every time on device start, but the input->buffer_p.count value is 0.
However, every time those callbacks have the same byte sequence (I inspected only the first byte in the buffer):
B8 9F D5 53 4B 08 F5 C5
Sometimes that callback sequence appear once, sometimes there is endlessloop. UART RX pin could be connected to some device or not - I always get that sequence and there is no valid transfer (I see some level changes on FX3 UART Rx pin, but no CyFxUSBUARTDmaCallback() calls and no data transfer to PC, of course).
Please explain the described situation. May be, I do something wrong.
Many thanks for help.
With regards,
Maksim
Show LessHello,
thanks to the help of this community my fx3 design is advancing quite well. Now I'm trying to configure the CTRL_COUNT in firmware rather than in the GPIF-Designer, since I want to be able to set the limit from my host application.
What I've done so far:
1. designed a state machine in the GPIF-Designer and added the LD_CTRL_COUNT action to a state, which is never reached. The counter is configured as an up-counter from 0 to 127. I had to do this, to be able to use the COUNT_CTRL action without errors in the GPIF-Designer
2. In the firmware, I've used the CyU3PGpifInitCtrlCounter() API to override the counter settings. For simplification I've just hardcoded the counter to run from 0 to 63. Later this value shall by configured via the host application before the GPIF is loaded/startet.
Based on the documentation, the CyU3PGpifInitCtrlCounter() API should override the counter configuration, but it does not work for me.
Show Less