USB Superspeed Peripherals

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
LBence91
USB Superspeed Peripherals
Hello! I am trying develop an UVC application with the FX3 board(CYUSB3KIT). I am using as a base the AN75779 document and the UVC_AN75779 example pro... Show More
louyuminghamn
USB Superspeed Peripherals
Hi,  There, We are using CYUSB3KIT-003 (the P/N of the chip is CYUSB3014) to design a camera. We need to send a leader and a trailer as single transfe... Show More
Myongho_Nov
USB Superspeed Peripherals
Hi. I'm  using CX3(CYUSB3065). When test using Stremer Program, the USB hub Operates normally. But Fail occurs when connecting directly to PC. How ca... Show More
SureshJ
USB Superspeed Peripherals
Hi, 1.Please confirm whether the AC capacitors are required between the Type-C connector and the MUX (PI5USB30213AXEA) input on TX lines. 2.Shall i ke... Show More
nluong
USB Superspeed Peripherals
Hello, I am trying to use the FX3 SlaveFIFO in 32-bit mode for automatic DMA transferring. I am able to fill up the buffers and send data to the host,... Show More
HuEl_264296
USB Superspeed Peripherals
On my CX3 board, the USBBulkSourceSink firmware example enumerates correctly, whether my board is is connected to a USB 3.0 or 3.2 socket. However, wh... Show More
Miquel
USB Superspeed Peripherals
Hi,   I am trying to program two different SPI nor flash memories using the Control Center. To do so, I want to use a GPIO from the FX3 to control a d... Show More
ZhaoYG
USB Superspeed Peripherals
I hope we can change the SPI  CPOL/ CPAH by a command from Host by any time . I can not find any examples like it. So i try to do it  by call CyU3PSpi... Show More
HuEl_264296
USB Superspeed Peripherals
This question is further to: Does the CX3 really need a clock buffer?  What are the drive requirements for the REFCLK and CLKIN pins on the CX3?  If I... Show More
zjjnsst
USB Superspeed Peripherals
连接了一块fpga 之前改成16位gpif的时候可以通过uvc在电脑上看到视频 但是我改成32位之后就变成黑屏了 然后接了串口看报错: …… Application StartedUVC: Completed 0 frames and 0 buffersDMA Reset Event: Frame ... Show More