USB superspeed peripherals Forum Discussions
text.format{('custom.tabs.no.results')}
Hello,
I want to know, what is the maximum size of Image file, that I can upload it to Denebola kit and run?
Hello,
I'm using this source https://community.infineon.com/t5/USB-superspeed-peripherals/CX3-Update-firmware-in-SPI-flash-over-HID-interface/m-p/118510
to update over HID, its totally working fine in USB 3.0, when I add HID interface for 2.0 in descriptors and plug it in 2.0, I'm facing some errors,
my DMA is resetting, what's the problem with DMA when I use HID in USB 2..0?
Show LessCan I run USBBulksourceSink and OV5640 example simultaneously in Denebolakit?
Hi,
I am implementing Fail Safe Firmware update which is referred here
I followed all instructions mentioned over there, but instead of using I2C I am using SPI flash. It is working fine with Fx3BootAppGcc and USBBulkSourceSink . But this time I am using Cx3UvcOV5640 instead of USBBulkSourceSink , I have included all the vendor commands part in Cx3UvcOV5640 . The Cx3UvcOV5640 task is being done properly but when I try to update the firmware using the FirmwareUpdate tool provided in the same link(above mentioned) it is not being done. I found that USB requests are not reaching Cx3UvcOV5640, so that vendor command part is not getting executed.
So, I want to know two things here
1. Why Cx3UvcOV5640 is unable to get USB request from host application?
2. Does Cx3UvcOV5640 only capable of receiving USB request from an UVC supported host application?
Thanks,
Abdul.
Show LessCyUSB3 USB Suite source is for revision 1.2.3.16.
Will source code for revision 1.2.3.20 (included in FX3 SDK) be available?
Dear community,
I encounter an issue with IO matrix initialization in the BulkLpAutoCpp example.
When I set the field useSpi to CyTrue, it never goes to CyFxApplicationDefine and the threads aren't launched.
It's working with other example but not this one.
I'd like to use both I2C & SPI. I'd like to use the Uart for debugging purpose.
Thank you for your help.
Show LessHello.
I have problem about download fx3sdksetup file from this site.
when download start look like normal. But when finish the file size is 2kb.
i try many way change i.e. browser, pc ,iPad but same problem.
this problem found on every download file. Except datasheet or pdf file.
how i can solved this problem.
Thankyou.
*sorry i’m not strong in english some word maybe missing spell.
* I already login as user of infineon site before download.
Show Less
How to make CX3 act as a bootloader device when it's pins are in SPI mode?
Does CX3 has efuse bootloader ?
If not, is there a plan to add the support to it? Is there an experimental driver that I can test with?