Whether CYUSB3065 CX3 can support S25FS128SAG and S25FS128SDS for SPI SDR and DDR mode

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Augustine_Yeh
Level 4
Level 4
Distributor - Zenitron(GC)
100 sign-ins 5 likes given 50 sign-ins

Hi Cypress

Whether CYUSB3065 CX3 can support S25FS128SAG and S25FS128SDS for SPI SDR and DDR mode ? Can we use  S25FS128SAG or S25FS128SDS with CYUSB3065 ?, If it can work , How about the SPI speed (If SPI speed is 33mhz)? Thank !!

0 Likes
1 Solution
JayakrishnaT_76
Moderator
Moderator
Moderator
First question asked 1000 replies posted 750 replies posted

Hello,

Please refer to the SPI timing diagrams (figure 10) in CX3 datasheet. From this, we can understand that DDR mode is not supported by CX3. Also, as you might be knowing the maximum operation frequency of SPI master of CX3 is 33MHz. Due to this the maximum interface speed with the flash will be 33MHz (even though the flash supports beyond this). So, both the flash parts S25FS128SAG and S25FS128SDS can be used with CX3 but in SDR mode only.

Best Regards,

Jayakrishna

Best Regards,
Jayakrishna

View solution in original post

0 Likes
1 Reply
JayakrishnaT_76
Moderator
Moderator
Moderator
First question asked 1000 replies posted 750 replies posted

Hello,

Please refer to the SPI timing diagrams (figure 10) in CX3 datasheet. From this, we can understand that DDR mode is not supported by CX3. Also, as you might be knowing the maximum operation frequency of SPI master of CX3 is 33MHz. Due to this the maximum interface speed with the flash will be 33MHz (even though the flash supports beyond this). So, both the flash parts S25FS128SAG and S25FS128SDS can be used with CX3 but in SDR mode only.

Best Regards,

Jayakrishna

Best Regards,
Jayakrishna
0 Likes