cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

arnova2
New Contributor II

We purchased a Terasic C5G FPGA board + FX3 Explorer Kit + Altera HSMC adapter board. According to Terasic's manual the voltage standard for the signals on the HSMC port is 2.5V. But on the FX3 Explorer Kit I can only select either 1.8V or 3.3V (with jumper J2). I already tried to find an answer in the Explorer Kit's manual but was unable to. The question is: What to do? Is the FX3 Explorer board 2.5V tolerant when set for 1.8V I/O operation? Afaik the C5G board is not 3.3V tolerant for 2.5V I/Os, right?

0 Likes
1 Solution
Rashi_Vatsa
Moderator
Moderator

Hello,

FX3 Explorer kit (CYUSB3KIT -003) doesn't have LDO for 2.5 V. We do not recommend to connect 2.5V I/O to 1.8 I/O of FX3

Please let me know if it is possible to change  the I/O level of the FPGA to 2.5V or can IOs with 3.3 V /1.8V be connected to FX3.

Regards,
Rashi

View solution in original post

0 Likes
2 Replies