- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi all,
I am building a USB device which needs to consume as less power as possible.
I was using Fx3s with SPI-Flash to boot the device, and the typical SPI-flash read current is about 10mA, while the F-RAM needs only 10 times less current.
Would it help to reduce the overall power consumption?
As there would be a 8-Mbits F-RAM coming, Is it possible to use it as the booting flash for Fx3S?
Thanks,
Jay
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Jay,
- The Excelon F-RAMs can be used as replacement for the SPI flash devices for booting. Upon looking into the datasheet of the Cypress Excelon F-RAM, the read/write commands are the same as in the case of FX3 supported SPI boot.
- SPI flash devices use the erase command before writing to the memory. But, F-RAMs do not require erasing. The Cypress Control Center issues the command to erase the SPI flash before write operation. The F-RAM ignores the command and hence the write operation will also be successful. In case, you are writing a custom vendor command in your firmware to write to the F-RAM, the erase command coming from the host must be handled without performing any SPI transfer.
Best regards,
Srinath S