- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In Cypress USB streamer example, when I use USB control center, select bulkin endpoint, then data transfer, transfer data in, for bytes to transfer, anything that is not a multiple of 1024 will result in
BULK IN transfer
BULK IN transfer failed with Error Code:997
For my own application, I want to do register read/write via USB to FPGA device in addition to streaming large amount of data. Is it possible to read/write data in multiple of 2*int32, instead of always asking for n*1024 bytes?
If that is not possible, what's the alternative solution? Can I create another two end points, that has maximum package size set to 8 bytes?
Thanks,
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
USB Bulk-in transfer can support any size of packets within the size of burst packets.
I understand you are using an FX3 example project supporting the Cypress USB streamer application.
I will use the USBBulkSourceSink (basic_example\cyfxbulksrcsink)
To make an 8-Byte packet at the FX3 firmware, Modify the CyFxBulkSrcSinkDmaCallback() function as follows.
if (type == CY_U3P_DMA_CB_CONS_EVENT)
{
/* This is a consume event notification to the CPU. This notification is
* received when a buffer is sent out from the device. We have to commit
* a new buffer as soon as a buffer is available to implement the data
* source. The data is preloaded into the buffer at that start. So just
* commit the buffer. */
status = CyU3PDmaChannelGetBuffer (chHandle, &buf_p, CYU3P_NO_WAIT);
if (status == CY_U3P_SUCCESS)
{
/* Commit the full buffer with default status. */
status = CyU3PDmaChannelCommitBuffer (chHandle, 8 /*buf_p.size*/, 0);
if (status != CY_U3P_SUCCESS)
{
CyU3PDebugPrint (4, "CyU3PDmaChannelCommitBuffer failed, Error code = %d\n", status);
}
}
else
{
CyU3PDebugPrint (4, "CyU3PDmaChannelGetBuffer failed, Error code = %d\n", status);
}
/* Increment the counter. */
glDMATxCount++;
}
Just change the second argument of the function call CyU3PDmaChannelCommitBuffer()
When you click the "Transfer Data-In" button you can see an 8-Byte packet is sent from FX3.
Please note that you will see six 16kB packets at first which is filled by the function CyFxBulkSrcSinkFillInBuffers()
Regards,
Noriaki