cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

masu_1341616
New Contributor II

Hello,

Is it possible to program SPI ROM for FX3 firmware without using Control Center? 

If don't have any solution from cypress, how about any third party product? 

Thanks

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator

Hello,

The SPI slave that is used should match the following write commands for successful programming from the USB Control Center.

  • Write Enable: 06h
  • Write data (Page Program): 02h
  • Sector Erase: D8h

In case the commands are different, the USB Control Center can be modified to suit the slave device that is used. The source of the control center can be found from the below path after the installation of FX3 SDK.

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\c_sharp\controlcenter

Best regards,

Srinath S

View solution in original post

0 Likes
1 Reply
SrinathS_16
Moderator
Moderator

Hello,

The SPI slave that is used should match the following write commands for successful programming from the USB Control Center.

  • Write Enable: 06h
  • Write data (Page Program): 02h
  • Sector Erase: D8h

In case the commands are different, the USB Control Center can be modified to suit the slave device that is used. The source of the control center can be found from the below path after the installation of FX3 SDK.

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\application\c_sharp\controlcenter

Best regards,

Srinath S

View solution in original post

0 Likes