- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear RSKV,
From the forum I found the post " http://www.cypress.com/?app=forum&id=167&rID=64701" and you helped clh23047 to resolve the debug issue.
Now I have the same question ,and after I read the DVK_guide.pdf , Syusb3014 datasheet and the post , I also can not resolve the issue. and my com also can not print logs.
I used the SDK sample "USBVideoclass" as the test project , I have checked the jumper connect , and it is right ! Then I connect the DVK and PC use COM ! and the source code you can refer to the SDK.
I have not changed the initial code about IO matrix . and then I add some "CyU3PDebugPrint(4, "Hello PC COM\n");" statements.
However, when I start the firmware used AMCAP, there are no logs print in "SecureCRT" . And I checked the settings of SecureCRT , the setting is "com1-115200-8-none-1".
Can you tell me why ?? Thanks !