Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
PraveenAmara
Level 2
Level 2
10 sign-ins 10 questions asked 5 sign-ins

I have to generate the PWM Signals from FX3 about 100 Hz to 5 kHz.

I have connected to Complex GPIF ( 18,19, 20, 21).

This is fine or I can generate the PWM from simple GPIF?

pastedImage_1.png

0 Likes
1 Solution
YashwantK_46
Moderator
Moderator
Moderator
100 solutions authored 50 solutions authored 50 likes received

Hi,

You can use the GIPO[18-21] as Complex GPIO's.

You can't use Simple GPIO's for generating PWM.


Please refer to section 8.9 of the FX3_TRM in the path for more information related to the GPIO's in FX3: C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\firmware\FX3_TRM.pdf

You can refer to 8.9.4.3 in section 8.9 for an example on configuring Complex GPIO to Generate PWM Output in FX3_TRM.pdf .

Regards,

Yashwant

View solution in original post

1 Reply
YashwantK_46
Moderator
Moderator
Moderator
100 solutions authored 50 solutions authored 50 likes received

Hi,

You can use the GIPO[18-21] as Complex GPIO's.

You can't use Simple GPIO's for generating PWM.


Please refer to section 8.9 of the FX3_TRM in the path for more information related to the GPIO's in FX3: C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\doc\firmware\FX3_TRM.pdf

You can refer to 8.9.4.3 in section 8.9 for an example on configuring Complex GPIO to Generate PWM Output in FX3_TRM.pdf .

Regards,

Yashwant