hello everybody,

   

i am working on interface between image sensor and FX3.

   

I used the description of example USBVideoClass and of course I modified sensor.c that allows to I2C to communicate with my Image sensor.

   

Of course, at the end I compile my app but these is a problem that occur.

   

I've attached screenshot of this problem on Eclipse. Thanks to help me

0 Likes
6 Replies
Anonymous
Not applicable

 Hi,

   

Please post the logs that appear in the Console Tab at the bottom. We can infer the cause of the errors from those logs.

   

Regards,

   

- Madhu Sudhan

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Ok.

   

I 've attached this

0 Likes
Anonymous
Not applicable

 Hi,

   

Open Command Prompt as Administrator and run the following command.

   

 cd "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\lib\gcc\arm-none-eabi"     

   

 

   

mklink /D 4.5.2 "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\ARM GCC\lib\gcc\arm-none-eabi\4.8.1"

   

Try compiling after you do this.

   

Regards,

   

- Madhu Sudhan

   

     

0 Likes
Anonymous
Not applicable

Ok. thanks it's done compulation success, what is the rule of those commands please ?

   

In fact there are few little warning, is it useful to consider those warnings ?

   

and then where could I get application (.img) to programm FX3  (which repository) ?

   

C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\\util\elf2img\elf2img.exe ? or not ? 

   

 I've atached the report and warnings that occur after compilation in pdf file.

0 Likes
Anonymous
Not applicable

Hello,

   

I resolved my problem about getting the .img (I took it in the debug file that is created after compilation) , yesterday.

   

But I want to know the target of this command...

   

regards,

   

sumarov

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

mklink creates in this case a link to a folder which accesses now the GCC version 4.8.1 under the name of the previous version 4.5.2.

   

 

   

Bob

0 Likes