- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I want to edit the driver inf file using the batch file listed in the question below, but I keep getting an error.
How can I fix it?
https://community.cypress.com/message/202697#202697
I am using windows10 64bit environment.
and i wanna add this string, but return error .
VID_04B4&PID_00F5.DeviceDesc="Cypress FX3 USB FPGA Device"
bat file result.
*******finding ProductType, 1=Work Station,
2= Domain Controller, 3= Server*******
ProductType is 1
IsClientOS is equal to true
64-bit
OSARCH is x64
OS Version is 10.0 and OS Name is Win10
"C:\PERSONAL_SPACE\2020년\SD_Configuration\FX3\CyUSB3_USB_Suite_Source\CYUSB3_1.2.3.20_BatchFile\CYUSB3_1.2.3.20_BatchFile"\Win10\x64
INFO:
Option set: dumping log info to console.
INFO:
Current working directory: 'C:\PERSONAL_SPACE\2020년\SD_Configuration\FX3\CyUSB3_USB_Suite_Source\CYUSB3_1.2.3.20_BatchFile\CYUSB3_1.2.3.20_BatchFile\Win10\x64'
INFO:
Running on path 'C:\PERSONAL_SPACE\2020년\SD_Configuration\FX3\CyUSB3_USB_Suite_Source\CYUSB3_1.2.3.20_BatchFile\CYUSB3_1.2.3.20_BatchFile\Win10\x64'
INFO:
No valid 'dpinst.xml' file provided.
INFO:
Install option set: Suppressing Wizard but no OS popups.
INFO:
Install option set: Suppressing EULA.
INFO:
Install option set: Force install if driver is not better.
INFO:
Install option set: Suppress Add or Remove Programs entries.
INFO:
Found driver package: 'C:\PERSONAL_SPACE\2020년\SD_Configuration\FX3\CyUSB3_USB_Suite_Source\CYUSB3_1.2.3.20_BatchFile\CYUSB3_1.2.3.20_BatchFile\Win10\x64\cyusb3.inf'.
INFO:
Preinstalling 'c:\personal_space\2020년\sd_configuration\fx3\cyusb3_usb_suite_source\cyusb3_1.2.3.20_batchfile\cyusb3_1.2.3.20_batchfile\win10\x64\cyusb3.inf'
...
INFO:
ENTER: DriverPackagePreinstallW
INFO:
RETURN: DriverPackagePreinstallW
(0xE000024B)
INFO:
Returning with code 0x80010000
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
Please refer to Part 2 Modifying CyUSB3.INF in the CyUSB.pdf from the FX3 SDK documents (path: <Fx3 installation directory>\EZ-USB FX3 SDK\1.3\doc\SuiteUSB)
Once the driver INF is modified, it needs to be signed to be installed by the dpinst tool.
Thanks,
Yatheesh