cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

JUTA_2823561
Contributor

I have a question about pin connections  on the CYUSB3610.

If not used, Wakeup# pin can be Open?

If not used, can MFA[2][3] pins be open?

If SUPER SUPEED is not used, can STMMX/P and SSRXM/P pins be open?

JUNYA

0 Likes
1 Solution
YashwantK_46
Moderator
Moderator

Hello Junya,

1.) If you don't need to implement an external wakeup, you can leave the WAKEUP# Unconnected/Open.

2.) MFA[2][3] can be left open, if not used.

3.) The SS lines can be left unconnected/open when not used.

Regards,
Yashwant

View solution in original post

0 Likes
1 Reply
YashwantK_46
Moderator
Moderator

Hello Junya,

1.) If you don't need to implement an external wakeup, you can leave the WAKEUP# Unconnected/Open.

2.) MFA[2][3] can be left open, if not used.

3.) The SS lines can be left unconnected/open when not used.

Regards,
Yashwant

View solution in original post

0 Likes