- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am Trying to receive image data coming from DDR3 to P-Port of FX3. From FX3 P-Port,i have to transfer it to S0 Port of FX3 and then to SD Card.
Which firmware is best suited for this application with better throughput?
Thanks in Advance.
Regards,
Srujana.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Srujana,
Please refer to the attached firmware. The default GpifToUsb firmware from the SDK is modified for functionality GPIF >SD card
The firmware supports GPIF to SD interface (without using MailBox registers unlike the example project in SDK), and can switch its role to SD to USB after receiving a vendor command.
There are different vendor commands used in the firmware you can choose the functionality as you need.( Refer to the comments in the file)
Please let me know if it helps
Regards,
Rashi
Rashi