cancel
Showing results for 
Search instead for 
Did you mean: 

USB Superspeed Peripherals

yogac_3765066
New Contributor II

Hello, everyone.


I'm new to FX3 and I needed to control GPIO ports from Host computer via USB vendor command.

I'm looking into examples but couldn't handle GPIO and USB transmission with computer simultaneously.

Any advice would be greatly appreciated.

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator

Hello,

For usage of GPIO control, refer to the GpioApp example that comes with the FX3 SDK. For implementation of vendor command, refer to the USBBulkSourceSink example. Combining these two, GPIO can be controlled over the vendor command issued from the host.

Best regards,

Srinath S

View solution in original post

2 Replies
SrinathS_16
Moderator
Moderator

Hello,

For usage of GPIO control, refer to the GpioApp example that comes with the FX3 SDK. For implementation of vendor command, refer to the USBBulkSourceSink example. Combining these two, GPIO can be controlled over the vendor command issued from the host.

Best regards,

Srinath S

View solution in original post

yogac_3765066
New Contributor II

Thank you, SrinathS_16

I'll try again with these examples.

And I'm looking forward to your support would be continued in the future.

PS: I'm not a native speaker. If there is misunderstanding, I am truly sorry.

Sincerely yours, Yondonjamts Ganzorig

0 Likes