Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I modified AN75779_001-75779_0B source code to interface FX3 with ZA10S20(1280x720/30fps/YUV422) of Zeeann Co.,Ltd.

   

I have a black screen, so I checked troubleshooting list in the AN75779.

   

I have checked the increasing frame counter using UART, It is ok.

   

I want to check next item, how to check the total amount of data being sent out per frame?

   

 

   

Many thanks.

   

MayFLY.

0 Likes
2 Replies
RaN_283461
Level 2
Level 2

Hi MayFLY

   

 In the if ((hitFV) && (prodCount == consCount)) block of UVC app thread entry you can print the producer count to see how many buffers were sent per frame , and also where the header for the last buffer is added you can print the produced_buffer.count to find the number of bytes in the last buffer.

   

But are you sure you dont get any commit buffer failures ??

   

Rags

0 Likes
Anonymous
Not applicable

Hi Rags,

   

Thanks for your reply.

   

I bought a PCI to USB3.0 host interface card, because my desktop PC does not have USB3.0.

   

I modified AN75779 souce code and build then dowload img to target board.

   

When I run virtualDub to check image, frame rate was 15.00fps and output size was 640x480.

   

At this time, I can see the buffer failures message through UART.

   

So, I modify source code for sensor to set VGA/15fps.

   

And try again, there was one or two buffer failures message before starting frame counting

   

and frame count value was increasing.

   

By the way, my board has a problem. Almost UART port is not work, sometimes is work.

   

so I just sent a email to customercare@cypress.com for asking after serive.

   

 

   

Many thanks.

   

BJ Lee.

0 Likes