- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi All,
I am working cypress FX3. I changed clock setting in GPIF designer to internal clock but I am getting 190MHz of frequency. How to set Clock internal Frequency range?.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The default clock values for the PIB block would be set to SYS_CLK/2, which would be 192MHz in case the SYS_CLK is 384MHz. To override this, modify the divider value in the CyU3PPibClock_t structure. Please use the following structure as parameter to the CyU3PPibInit() API.
pibClock.clkDiv = 4; // Clock divider is set to 4.
//Modify this value to generate different clock frequencies
pibClock.clkSrc = CY_U3P_SYS_CLK; // Clock frequency is derived from the SYS_CLK
pibClock.isHalfDiv = CyFalse;
/* Disable DLL for sync GPIF */
pibClock.isDllEnable = CyFalse;
The above structure will generate a clock frequency of 100.8MHz (maximum supported on the GPIF II interface) if the SYS_CLK frequency is chosen to 403.2MHz.
Best regards,
Srinath S