- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi All:
I referred the AN75779 document to achieve the UVC device, and it works!
However, I met a trouble to define the Camera Terminal - Exposure Time (Absolute) Control.
I don’t know how to define that... It’s more difficult than the Processing Unit, such as Brightness Control.
I also refer the “USB Device Class Definition for Video Devices v1.5.pdf” for the control function, but it don’t describe the rule detailed.
Now I just know the Exposure Time (Absolute) Control is defined by “2 to the power of n”, and the resolution(one step) is to change the “n”.
[Goat]
Total Step: 10(-10 ~ -1)
Max value: 1024
Min value: 1
Default value: 256
[My Setting]
[My Result]
It’s strange... (Checked the actual setting value by UART)
The slider range: -13 ~ -3
Max value: 1024
Min value: 1
Each step value
Hope somebody could provide me some suggestions, or provide an example by my [Goat].
Thank you so much!
Hughes
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
hello,
Windows using log2() second to get/set exposure time.
Your max/min value (4/2) means 0.4ms and 0.2ms,
and
log2(0.0004) = -11.28771,
log2(0.0002) = -12.28771.
so the result is -11 and -12.
KSPROPERTY\_CAMERACONTROL\_EXPOSURE - Windows drivers | Microsoft Docs
Hope this helps.