- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm using a CYUSB3KIT to transfer 32-bit width data from another data source device.
Configuration is:
The FX3 works as a slave, and the external data source device is the master. The interface's clock rate is 75M, generated from master. The interface is one-direction, data transfer from external to FX3 only. There is no write enable signal, so the validity of data is controlled by disabling the clock at master. Two flags are used. One is TH0 ready, one is TH0 WM. State machine only have one DMA channel, always use TH0 to send and wait if TH0_READY is not active.
Problem is :
The master stops sending clock edges when READY or WM is not active, but the two signals will not be active forever. if I force the master to send clocks, after sending about 32 clocks, the two signals are valid.
And for more, I found that the polarity of these two signals are reversed to the setting in GPIF. The signal is set to be active high, but measured to be active low (by forcing the master to send clocks without receive from host, the two signals should be not ready).
Do the flags need continuous clock? Is that the reason why the flags stuck?
Best Regards,
W.D.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I would suggest you to provide free running clock on the PCLK line and use one control signal to assert when the DMA RDY flag is HIGH to sample the data to FX3,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I would suggest you to provide free running clock on the PCLK line and use one control signal to assert when the DMA RDY flag is HIGH to sample the data to FX3,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you! I tried it and it works! The Ready and WM signals do not act if there is no clock